Robot monitoring idea using #freemasterdash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Robot monitoring idea using #freemasterdash

1,902 Views
fred27murphy
Contributor II

I've got a current project where I need to monitor the state of a number of industrial robots such as is the e-Stop has been triggered. I also need to stop and start them remotely.

I was initially going to host a very simple UI on an FRDM-K64F, but FreeMASTER seems like a good fit for creating a nicer UI for this process - including status indicators and controls. I've spent many years as a web developer so will probably use custom code rather than relying on 3rd party widgets.

0 Kudos
Reply
1 Reply

1,834 Views
MichalH
NXP Apps Support
NXP Apps Support

Dear Fred,

this is a great plan. I can't wait to see the result. In case of any problem with JSON-RPC API or FreeMASTER interfacing, don't hesitate to submit a question to this forum.

Thank you,

Michal

0 Kudos
Reply