Problems with incorrect freemaster Recorder data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with incorrect freemaster Recorder data

Jump to solution
6,257 Views
zyyy
Contributor I

freemaster had been using version 2.0 before, and later updated to version 3.0, the Recorder data became incorrect

Tags (2)
0 Kudos
Reply
1 Solution
6,212 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello,

by using NXP FreeMASTER with microcontrollers from other vendor you are violating FreeMASTER license conditions. You have agreed with the conditions when downloading and then also when installing the FreeMASTER.

You can only use FreeMASTER with NXP MCUs.

 

View solution in original post

0 Kudos
Reply
3 Replies
6,242 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello,

we would need more information about the issue like:

  • Exact version of the FreeMASTER tool (the latest is 3.2.4, see Help/About)
  • What is the target MCU?
  • What communication and driver software is used at the MCU side? (the latest can be found in various SDK packages or at GitHub)
  • What do you mean by incorrect data?

Thank you,
Michal

0 Kudos
Reply
6,213 Views
zyyy
Contributor I

Hello,

I am using Freemaster version 3.2.4.3

Using STM32F103 MCU

Uart communication used on MCU end

The data in Figure 3 on the left appears to be incorrect and is using version 3.0, while the data in Figure 2 on the right is normal and is using version 2.0

0 Kudos
Reply
6,212 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello,

by using NXP FreeMASTER with microcontrollers from other vendor you are violating FreeMASTER license conditions. You have agreed with the conditions when downloading and then also when installing the FreeMASTER.

You can only use FreeMASTER with NXP MCUs.

 

0 Kudos
Reply