PCAN Driver for Freemaster

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCAN Driver for Freemaster

6,231件の閲覧回数
Bohrfutter
Contributor III

Hello

I want to share my DLL to use PEAK CAN2USB adapter with Freemaster CAN Plugin. You have to store the attached files under \FreeMASTER 2.0\plugins\can. Now you can select the ZLG device and select ControlPCAN.dll. If things are working you should have a ZLG 3.0 device which is the PCAN USB2CAN adapter.

Update: Removed the attachment - PCAN support will be part of the next Freemaster release.

Have fun

Sebastian

0 件の賞賛
返信
5 返答(返信)

6,057件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Dear Sebastian,

thank you for sharing this experience, we are going to add official PCAN support to the next release. For now, please remove the attachments from your post as it is not clear what license is used and if you are permitted to make the files available openly. 

Thank you,

Michal

0 件の賞賛
返信

6,057件の閲覧回数
Bohrfutter
Contributor III

Hello Michal,

is there already a planed release date?

The PCanBasic.dll can be shared ( PEAK-System Forum • View topic - PCAN License coverage for opening Open source ) and I wrote the ControlPCAN.dll - anyway I removed the two files for not having any legal problems. If it is helping I can share the source code of the ControlPCAN.dll so implementation of PCAN maybe less painful...

Cheers

Sebastian

0 件の賞賛
返信

4,173件の閲覧回数
superbit
Contributor I

Can you share it with me
Email: [email protected]
Thank you.

0 件の賞賛
返信

6,057件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

I'm sorry the next release is not yet planned.

0 件の賞賛
返信

6,057件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

OK, I did not know that the ControlPCAN.dll is your work. Good job! But anyway, we should not need this library as the CAN plug-in will interface to PCanBasic.dll directly. Thanks again.

0 件の賞賛
返信