Is it possible to get a symbol data type using the ActiveX API?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to get a symbol data type using the ActiveX API?

ソリューションへジャンプ
4,173件の閲覧回数
lucabarbiero
Contributor IV

Hi,

The ActiveX API provides a method GetSymbolInfo, which returns address and size for an input symbol name.

But I also need the data type, and I don't see any API feature to get this info.

I am using TSA tables in my embedded application, so I would expect the data type information to be available to the host.

Do you confirm this feature is missing?

 

Regards,

Luca

 
 

 

 

0 件の賞賛
返信
1 解決策
4,141件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello Luca,

you should be able to use GetSymbolInfo on the array symbol to retrieve its byte-wise size. Then you can use GetSymbolInfo on the array[0] symbol to retrieve a size of one element. Dividing the two should give you a count.

Regards,
Michal

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,144件の閲覧回数
lucabarbiero
Contributor IV

Hi Michal,

If I may add to the backlog, it would be good to also get the length info for arrays through the API. When I generate FreeMASTER variables from an array symbol using the Windows app, it knows the length of arrays and it can generate as many variables as the number of array elements.

Just getting the length info and the start address via API would enable me to script something similar.

 

Regards,

Luca

0 件の賞賛
返信
4,142件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello Luca,

you should be able to use GetSymbolInfo on the array symbol to retrieve its byte-wise size. Then you can use GetSymbolInfo on the array[0] symbol to retrieve a size of one element. Dividing the two should give you a count.

Regards,
Michal

0 件の賞賛
返信
4,136件の閲覧回数
lucabarbiero
Contributor IV

Ok understood, that is the trick. Thanks!

0 件の賞賛
返信
4,169件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello Luca,

I confirm this is not possible with the current version, the GetSymbolInfo only returns address and size of the symbol or it evaluates a complex expression similarly as the Variable definition dialog does. Note that this evaluation may access multiple symbols (e.g. there can be a mix of symbol names and multiple  sizeof(x) and valueof(z) operators). This is why it is not just one symbol whose name we would return.

But I agree that in most of the cases, you are just interested in a simple symbol name lookup and in this case, returning the type name is a good idea. Added to backlog for 3.2.2 (also for GetAddressInfo).

Thanks,
Michal