How to show Matrix array on Freemaster

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to show Matrix array on Freemaster

1,550件の閲覧回数
Davidino
Contributor IV

Goodmorning,

I'm using Freemaster version 3.2.0.5 succesfully, except for the following struct:

 

typedef struct
{
    DIRECTION direction;                                           				
    int16_t encoderEventImpulses[ARRAY_SIZE_MOTORS][MAX_NUM_OF_ENCODER_EVENT+1];          						
    bool encoderEventEnable[ARRAY_SIZE_MOTORS][MAX_NUM_OF_ENCODER_EVENT+1];
    uint16_t encoderEventSize[ARRAY_SIZE_MOTORS];                                          						
    int16_t angleLoaded[ARRAY_SIZE_MOTORS];																		

    bool changeSign;																							
    uint16_t angleEnabledCounter;										
    uint16_t angleUsableIndex;										
	NUMMOT motorNum;								
	uint16_t numOfEncoderCompareAngleChangedListener[ARRAY_SIZE_MOTORS];		
}tEncoderEvent;

 

As you can see some struct members, such as encoderEventImpulses, are array matrixes.

How can I show this kind of values on Freemaster?

Thank you in advanced.

Davidino

0 件の賞賛
返信
0 返答(返信)