How to deal with a null Plugin-Module in FREEMASTER?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to deal with a null Plugin-Module in FREEMASTER?

ソリューションへジャンプ
3,705件の閲覧回数
William-Lee
Contributor II

I had installed the freemaster 3.1,and I want to use the PE-micro to monitor variables ,but the Plugin-Module is NULL.Do I need to install something else?Is there any body meet this situation?please give me a hand , thanks a lot .福昕截屏20220715105304376.PNG

0 件の賞賛
返信
1 解決策
3,700件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello,

probably there was some problem for the installer to acquire administrator rights during installation. You should be able to fix it by running the "c:\NXP\FreeMASTER 3.1\FreeMASTER\register.bat" as administrator.

If this does not help, please re-install the FreeMASTER. First un-install the product and then install again by running the installer "as administrator".

MichalH_0-1657868496713.png

Regards,
Michal

元の投稿で解決策を見る

2 返答(返信)
3,701件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello,

probably there was some problem for the installer to acquire administrator rights during installation. You should be able to fix it by running the "c:\NXP\FreeMASTER 3.1\FreeMASTER\register.bat" as administrator.

If this does not help, please re-install the FreeMASTER. First un-install the product and then install again by running the installer "as administrator".

MichalH_0-1657868496713.png

Regards,
Michal

3,674件の閲覧回数
William-Lee
Contributor II

It works, thanks for your help!

0 件の賞賛
返信