Handle a recorder in JS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Handle a recorder in JS

4,031 Views
FaustoPignatta
Contributor I

Hi,

there is an example that describes how to implement a recorder in JS scripting?

Many thanks

 

Fausto

0 Kudos
Reply
6 Replies

4,023 Views
FaustoPignatta
Contributor I

Hi Daniel,

I'm using Freemaster to create a debug page of my application (that runs on s32k148 micro). I have created an html page and use JS scripting.

I've tried to use this function

PCM.prototype.SetupRecorder = function(id, config, vars)... (freemaster-client.js)
 
without success.
 
Many thanks,
 
Fausto
0 Kudos
Reply

4,002 Views
iulian_stan
NXP Employee
NXP Employee

Hi @FaustoPignatta,

Are you using FreeMASTER (GUI tool) or FreeMASTER Lite as a backend for html page ?

I am asking because SetupRecorder is a special case - specific to FreeMASTER Lite (won't work with main FreeMASTER tool). The GUI tool has an alternative function DefineRecorder (6.5.41 User Manual).

Depending on your use case we will provide a corresponding example.

Regards,
Iulian

0 Kudos
Reply

4,000 Views
FaustoPignatta
Contributor I

Hi Iulian,

I'm using Freemaster (Gui Tool), and i put in my project these files (like I see in scripting example ..\FreeMASTER 3.0\FreeMASTER\examples\scripting\JavaScript-JSON-RPC):

- freemaster-client.js 

- simple-jsonrpc.js

 

Thanks

Fausto

0 Kudos
Reply

3,995 Views
MichalH
NXP Apps Support
NXP Apps Support

Dear Fausto,

The Oscilloscope is more a user-interactive feature than a programmatic one in the FreeMASTER Desktop application. There is actually no JSON-RPC API to consume oscilloscope data in the script as such script would depend heavily on what oscilloscope item is currently selected in the project tree. 

There is an API though to create the Oscilloscope item and populate it with selected variables just like if the user would create it by hand. There is also an API to activate the newly created item in the project tree so that the oscilloscope graph becomes visible in the desktop window. See DefineOscilloscope and SelectItem API calls in the User Guide.

In the FreeMASTER Desktop application, the only way how to get variable values in run-time is reading them programmatically in a script using the ReadVariable or similar methods. This is a good approach as it works any time, regardless of what screen the user currently activates in the UI.

As Iulian mentioned above, the FreeMASTER Lite backend enables an access to Oscilloscope feature at the protocol level, so it might be more suitable for you if you really need a high-speed data sampling.

Regards,
Michal

0 Kudos
Reply

3,992 Views
FaustoPignatta
Contributor I

Hi Michal,

thanks for the suggestion. I've declared some array MCU side and read them in my desktop application with pcm.ReadUIntArray function. In my application I don't need to see real time values but only to acquire them in the fastest way, and at the end of process analyze them.

Thanks,

Fausto

0 Kudos
Reply

4,025 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Which NXP product do you use?

 

Thanks,

BR, Daniel

0 Kudos
Reply