Getting started with S32K146EVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Getting started with S32K146EVB

ソリューションへジャンプ
2,291件の閲覧回数
Meneglier
Contributor I

Hello, I have some difficulty with the board S32K146EVB when I try to use the demo application FreeMASTER like the quick start guide :

The board is well connected with port com3 : 115000 bd

The JumpStart project will be automaticaly downloaded from www.nxp.com Once the FreeMASTER application detects the web address stored as an TSA active content in the flash memory of the S32K146 MCU, the download of the FreeMASTER project from www.nxp.com will be initiated.

A error message appear :

Meneglier_0-1678357684175.png

 

0 件の賞賛
返信
1 解決策
2,191件の閲覧回数
iulian_stan
NXP Employee
NXP Employee

The URL issue was fixed, updated firmware can be downloaded from S32K146 product page.

FreeMASTER (PC) project is also available on the same page for offline mode.

Capture.PNG

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,280件の閲覧回数
iulian_stan
NXP Employee
NXP Employee

Hi @Meneglier,

Please find attached FreeMASTER project.
Open it directly in FreeMASTER tool, then connect to your board. 

Kind regards,
Iulian

0 件の賞賛
返信
2,192件の閲覧回数
iulian_stan
NXP Employee
NXP Employee

The URL issue was fixed, updated firmware can be downloaded from S32K146 product page.

FreeMASTER (PC) project is also available on the same page for offline mode.

Capture.PNG

 

0 件の賞賛
返信