Getting started with S32K146EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting started with S32K146EVB

Jump to solution
2,308 Views
Meneglier
Contributor I

Hello, I have some difficulty with the board S32K146EVB when I try to use the demo application FreeMASTER like the quick start guide :

The board is well connected with port com3 : 115000 bd

The JumpStart project will be automaticaly downloaded from www.nxp.com Once the FreeMASTER application detects the web address stored as an TSA active content in the flash memory of the S32K146 MCU, the download of the FreeMASTER project from www.nxp.com will be initiated.

A error message appear :

Meneglier_0-1678357684175.png

 

0 Kudos
Reply
1 Solution
2,208 Views
iulian_stan
NXP Employee
NXP Employee

The URL issue was fixed, updated firmware can be downloaded from S32K146 product page.

FreeMASTER (PC) project is also available on the same page for offline mode.

Capture.PNG

 

View solution in original post

0 Kudos
Reply
2 Replies
2,297 Views
iulian_stan
NXP Employee
NXP Employee

Hi @Meneglier,

Please find attached FreeMASTER project.
Open it directly in FreeMASTER tool, then connect to your board. 

Kind regards,
Iulian

0 Kudos
Reply
2,209 Views
iulian_stan
NXP Employee
NXP Employee

The URL issue was fixed, updated firmware can be downloaded from S32K146 product page.

FreeMASTER (PC) project is also available on the same page for offline mode.

Capture.PNG

 

0 Kudos
Reply