Freemaster: Stopped, waiting for acknowledgement

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Freemaster: Stopped, waiting for acknowledgement

跳至解决方案
6,674 次查看
Sam_ECU
Contributor V

Hello @MichalH

As discussed in the post below, when using the recorder in Freemaster I receive the message "Stopped, waiting for acknowledgement" once the measurement is finished.  I then don't get any results.

https://community.nxp.com/t5/FreeMASTER/FreeMASTER-3-0-Problem-with-the-Recorder/m-p/1447668#M971

Sam_ECU_1-1650626801088.png

 

I'm working with the MCU below:

Sam_ECU_0-1650626754627.png

I'm using the latest version of Freemaster:

Sam_ECU_2-1650626856679.png

How can I resolve the issue?

Thanks for the help,

Sam

标记 (2)
0 项奖励
回复
1 解答
6,635 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello Sam,

In general, a similar recorder behavior can be seen when FMSTR_Recorder() is not called periodically by the MCU application - so its state machine is not running. 

I see that you use the Matlab Model-based design toolbox. I'm not an expert here, but I think the "Recorder Call" should be put in a block which is triggered periodically, e.g. by an interrupt. You can check the generated C code to see how is the FMSTR_Recorder() called.

I also recommend to refer to a MBDT Motor Control demo which makes use of an interrupt-driven recorder. If you need a further help, I will ask someone from MBDT team to step in. 

Regards,
Michal

 

 

在原帖中查看解决方案

0 项奖励
回复
5 回复数
6,636 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello Sam,

In general, a similar recorder behavior can be seen when FMSTR_Recorder() is not called periodically by the MCU application - so its state machine is not running. 

I see that you use the Matlab Model-based design toolbox. I'm not an expert here, but I think the "Recorder Call" should be put in a block which is triggered periodically, e.g. by an interrupt. You can check the generated C code to see how is the FMSTR_Recorder() called.

I also recommend to refer to a MBDT Motor Control demo which makes use of an interrupt-driven recorder. If you need a further help, I will ask someone from MBDT team to step in. 

Regards,
Michal

 

 

0 项奖励
回复
6,633 次查看
Sam_ECU
Contributor V

Hello Michal,

I had it located within an atomic system, that appears to have been the issue.

Thanks,

Sam

0 项奖励
回复
4,692 次查看
Xiaowei_Chu
Contributor I
Hello Sam,
Would you please share the detail information about how you solve the issue. I met the same issue in MBDT.
0 项奖励
回复
4,626 次查看
Sam_ECU
Contributor V

It's been awhile but I believe the Recoder-Block needed to be on the front page of Simulink and not within any function or atomic blocks.

0 项奖励
回复
6,625 次查看
MichalH
NXP Apps Support
NXP Apps Support

OK, thanks for info. Please mark the answer above as 'correct' to close this thread.

Thank you,
Michal

0 项奖励
回复