Freemaster Recorder Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freemaster Recorder Error

1,855件の閲覧回数
osmanyucel
Contributor I

I created a recorder but it does not work. There is an error 0x80000081(invalid command). I added FMSTR_Recorder(0) also.

0 件の賞賛
返信
1 返信

1,833件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello, 

you do not write what communication interface you are using. Please note that Recorder does not run over JTAG and BDM direct memory access.

In case you use UART, CAN, USB-CDC, Ethernet or JTAG PD-BDM or RTT, the recorder should work. Please make sure you have the recorder enabled in freemaster_cfg. by setting FMSTR_USE_RECORDER 1  (or 2, 3, ... depending on number of recorders you need to run simultaneously).

Regards,
Michal 

0 件の賞賛
返信