Freemaster Query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freemaster Query

2,245 Views
21
Contributor I

When I open MC9S12ZVML128_BLDC_Hall.pmp with FreeMASTER3.0, the following prompt appears. How do I solve this problem?
Error show-
1.symbol not found.
2.communication Error.
3.If started the communication then, not getting the values if variable 

0 Kudos
Reply
2 Replies

2,188 Views
21
Contributor I

Yes, BLDC app is loaded in the target MCU Board.
PC through code worrier BLDC application code is loaded on MCU board through P&E debugger and then connect MCU board USB/SCI free master to PC through USB and opening project in Free master and starting Communication. There is communication error is show.

0 Kudos
Reply

2,233 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello,

do you have the BLDC application loaded in the target MCU board and is the board properly connected to the PC?

Please describe your hardware setup, what application you run in the MCU and how is your PC connected to the board.

Thanks,
Michal

0 Kudos
Reply