Freemaster Protocol on CAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freemaster Protocol on CAN

ソリューションへジャンプ
5,245件の閲覧回数
nxf64554
NXP Employee
NXP Employee

Hi, Is there any documentation about how Freemaster protocol is encoded (i.e. in CAN messages)?

I am trying to understand the low level of the communication driver code so I might be able to modify it for a specific application.

Thanks!

1 解決策
5,141件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Dear Weilin Cao,

the FreeMASTER-over-CAN protocol uses the same command/response format as a "native" Serial protocol. The payload is split to 7-byte chunks and is transmitted over a simple CAN signalling protocol. I'm attaching a white paper which describes general concepts of both Serial protocol and also the CAN transport.

Best regards,

Michal

元の投稿で解決策を見る

2 返答(返信)
5,142件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Dear Weilin Cao,

the FreeMASTER-over-CAN protocol uses the same command/response format as a "native" Serial protocol. The payload is split to 7-byte chunks and is transmitted over a simple CAN signalling protocol. I'm attaching a white paper which describes general concepts of both Serial protocol and also the CAN transport.

Best regards,

Michal

5,140件の閲覧回数
nxf64554
NXP Employee
NXP Employee

Thanks that is exactly what I am looking for!

0 件の賞賛
返信