Freemaster 3.1 - example project with MCUXpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freemaster 3.1 - example project with MCUXpresso

1,811件の閲覧回数
rt54321
Contributor I

Greetings!

Using FreeMaster 3.1 with the RT1010EVK and MCUXpresso.  In my SDK, I have download the FreeMaster example uart application, and it runs on my RT1010EVK board.

In FreeMaster, I can connect to the board through the "Connection Wizard" with the simple serial port.  Now, what can I "do" in FreeMaster?  Is there an example tutorial that shows how to view/add the cariables in the firmware to FreeMaster?  Is there a ready-made FreeMaster project that I can load with this SDK example?

 

0 件の賞賛
返信
1 返信

1,797件の閲覧回数
iulian_stan
NXP Employee
NXP Employee

Hi @rt54321,

In the root folder of your project you will find a corresponding FreeMASTER project (`.pmp` file).

Capture.PNG

 

There is a basic example on FreeMASTER usage available in this article (video). A more extensive example about FreeMASTER features can be found here (webinar VOD).

Regards,
Iulian

 

0 件の賞賛
返信