FreeMASTER source codes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeMASTER source codes

Jump to solution
3,444 Views
stepan_podhorsk
Contributor II

Hello,

please can anybody tell me whether the source codes for the FreeMASTER software are available for download? Thanks.

Tags (2)
0 Kudos
Reply
1 Solution
3,339 Views
MichalH
NXP Apps Support
NXP Apps Support

Dear Stepan,

the source code of FreeMASTER serial and CAN communication driver is available in the MCUXpresso SDK. The source code is the same for all MCUs supported by the SDK, so just pick any of the supported devices or boards (e.g. FRDM-K64F) and add the FreeMASTER  middleware component. The sources will be located in middleware/freemaster directory in the generated SDK ZIP package. 

If you ask about sources of the FreeMASTER desktop applications, then the answer is no. The sources are not publicly available.

Best regards,

Michal

View solution in original post

0 Kudos
Reply
1 Reply
3,339 Views
MichalH
NXP Apps Support
NXP Apps Support

Dear Stepan,

the source code of FreeMASTER serial and CAN communication driver is available in the MCUXpresso SDK. The source code is the same for all MCUs supported by the SDK, so just pick any of the supported devices or boards (e.g. FRDM-K64F) and add the FreeMASTER  middleware component. The sources will be located in middleware/freemaster directory in the generated SDK ZIP package. 

If you ask about sources of the FreeMASTER desktop applications, then the answer is no. The sources are not publicly available.

Best regards,

Michal

0 Kudos
Reply