Error when opening project in FreeMaster

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error when opening project in FreeMaster

2,933 Views
niels_steyaert
Contributor I

Hello

I was following this guide (https://www.nxp.com/docs/en/application-note/AN12709.pdf ) to set up the FRDM-TOUCH, but I can't solve the error message appearing in step 7.3. 

When importing the project file this message appears:

pastedImage_2.png

The board (FRDM-KE15Z) is successfully discoverd and connected in FreeMaster. 

This error looks like this: get error to load freemaster project on PMSM with RT1050  , but nothing helped.

I tried a different pc, with the same error.

I tried Freemaster 3.0 & 2.5.

What can I do next?

Thx!

0 Kudos
Reply
3 Replies

2,816 Views
iulian_stan
NXP Employee
NXP Employee

Hi [email protected]‌,

It looks like the project uses some relative paths that are resolved with respect to .pmp file location (not the temporary folder - the one you see in the message box). To fix this one I've done the following:

  • moved temporary directory content into the src folder next to .pmp file.

Capture.PNG

If you navigate to Project→Options...→Pack Dir, you will see that it's the original resource folder.

Capture.PNG

Hope this helps,

Iulian

2,816 Views
niels_steyaert
Contributor I

Hi Lulian

Thanks for the answer!

This helped, I can now open the project without error's.

But, now I'm stucked at an other issue:

When pressing the "READ CONFIGURATION FROM BOARD", this message appears:

pastedImage_1.png

Following by this:

pastedImage_2.png

In the debug panel it looks like this:

NXP Touch GUI Tool | NXP

can not find symbol info "_nt_system.time_period"

Symbol _nt_system.time_period not found.Symbol not found (_nt_system.time_period).

can not find symbol info "_nt_system.init_time"

Symbol _nt_system.init_time not found.Symbol not found (_nt_system.init_time).

can not find symbol info "_nt_system.safety_period_multiple"

Symbol _nt_system.safety_period_multiple not found.Symbol not found (_nt_system.safety_period_multiple).

can not find symbol info "_nt_system.safety_crc_hw"

Symbol _nt_system.safety_crc_hw not found.Symbol not found (_nt_system.safety_crc_hw).

can not find symbol info "nt_kernel_data.modules[0]->rom->wtrmark_hi"

Symbol nt_kernel_data.modules[0]->rom->wtrmark_hi not found.Symbol not found (nt_kernel_data.modules[0]->rom->wtrmark_hi).

can not find symbol info "nt_kernel_data.modules[0]->rom->wtrmark_lo"

Symbol nt_kernel_data.modules[0]->rom->wtrmark_lo not found.Symbol not found (nt_kernel_data.modules[0]->rom->wtrmark_lo).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.mainClock"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.mainClock not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.mainClock).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.ssc_mode"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.ssc_mode not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.ssc_mode).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.mode"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.mode not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.mode).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.dvolt"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.dvolt not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.dvolt).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.cutoff"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.cutoff not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.cutoff).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.order"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.order not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.order).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.decimation"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.decimation not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.decimation).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.chargeNum"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.chargeNum not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.chargeNum).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.prbsOutsel"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.prbsOutsel not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.prbsOutsel).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.noChargeNum"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.noChargeNum not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.noChargeNum).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.ssc_prescaler"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.ssc_prescaler not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.commonConfig.ssc_prescaler).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.enableSensitivity"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.enableSensitivity not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.enableSensitivity).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.enableShield"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.enableShield not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.enableShield).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.xdn"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.xdn not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.xdn).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.ctrim"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.ctrim not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.ctrim).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.inputCurrent"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.inputCurrent not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.inputCurrent).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configSelfCap.chargeCurrent"

Symbol nt_kernel_data.modules[0]->rom->config->configSelfCap.chargeCurrent not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configSelfCap.chargeCurrent).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.mainClock"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.mainClock not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.mainClock).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.ssc_mode"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.ssc_mode not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.ssc_mode).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.mode"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.mode not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.mode).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.dvolt"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.dvolt not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.dvolt).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.cutoff"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.cutoff not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.cutoff).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.order"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.order not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.order).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.decimation"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.decimation not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.decimation).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.chargeNum"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.chargeNum not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.chargeNum).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.noChargeNum"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.noChargeNum not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.noChargeNum).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.prbsOutsel"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.prbsOutsel not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.prbsOutsel).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.ssc_prescaler"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.ssc_prescaler not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.commonConfig.ssc_prescaler).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.preCurrent"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.preCurrent not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.preCurrent).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.preResistor"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.preResistor not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.preResistor).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.senseResistor"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.senseResistor not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.senseResistor).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.boostCurrent"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.boostCurrent not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.boostCurrent).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.txDriveMode"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.txDriveMode not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.txDriveMode).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.pmosLeftCurrent"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.pmosLeftCurrent not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.pmosLeftCurrent).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.pmosRightCurrent"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.pmosRightCurrent not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.pmosRightCurrent).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->configMutual.enableNmosMirror"

Symbol nt_kernel_data.modules[0]->rom->config->configMutual.enableNmosMirror not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->configMutual.enableNmosMirror).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->thresl"

Symbol nt_kernel_data.modules[0]->rom->config->thresl not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->thresl).

can not find symbol info "nt_kernel_data.modules[0]->rom->config->thresh"

Symbol nt_kernel_data.modules[0]->rom->config->thresh not found.Symbol not found (nt_kernel_data.modules[0]->rom->config->thresh).

can not find symbol info "nt_kernel_data.modules[0]->rom->instance"

Symbol nt_kernel_data.modules[0]->rom->instance not found.Symbol not found (nt_kernel_data.modules[0]->rom->instance).

can not find symbol info "nt_kernel_data.modules[0]->rom->safety_params.gpio->delay_interval"

Symbol nt_kernel_data.modules[0]->rom->safety_params.gpio->delay_interval not found.Symbol not found (nt_kernel_data.modules[0]->rom->safety_params.gpio->delay_interval).

can not find symbol info "nt_kernel_data.modules[0]->rom->recalib_config->SelfRangeMin"

Symbol nt_kernel_data.modules[0]->rom->recalib_config->SelfRangeMin not found.Symbol not found (nt_kernel_data.modules[0]->rom->recalib_config->SelfRangeMin).

can not find symbol info "nt_kernel_data.modules[0]->rom->recalib_config->SelfRangeMax"

Symbol nt_kernel_data.modules[0]->rom->recalib_config->SelfRangeMax not found.Symbol not found (nt_kernel_data.modules[0]->rom->recalib_config->SelfRangeMax).

can not find symbol info "nt_kernel_data.modules[0]->rom->recalib_config->SelfRangeDeltaMin"

Symbol nt_kernel_data.modules[0]->rom->recalib_config->SelfRangeDeltaMin not found.Symbol not found (nt_kernel_data.modules[0]->rom->recalib_config->SelfRangeDeltaMin).

can not find symbol info "nt_kernel_data.modules[0]->rom->recalib_config->SelfRangeDeltaMax"

Symbol nt_kernel_data.modules[0]->rom->recalib_config->SelfRangeDeltaMax not found.Symbol not found (nt_kernel_data.modules[0]->rom->recalib_config->SelfRangeDeltaMax).

can not find symbol info "nt_kernel_data.modules[0]->rom->recalib_config->MutRangeMin"

Symbol nt_kernel_data.modules[0]->rom->recalib_config->MutRangeMin not found.Symbol not found (nt_kernel_data.modules[0]->rom->recalib_config->MutRangeMin).

can not find symbol info "nt_kernel_data.modules[0]->rom->recalib_config->MutRangeMax"

Symbol nt_kernel_data.modules[0]->rom->recalib_config->MutRangeMax not found.Symbol not found (nt_kernel_data.modules[0]->rom->recalib_config->MutRangeMax).

can not find symbol info "nt_kernel_data.modules[0]->rom->recalib_config->MutRangeDeltaMin"

Symbol nt_kernel_data.modules[0]->rom->recalib_config->MutRangeDeltaMin not found.Symbol not found (nt_kernel_data.modules[0]->rom->recalib_config->MutRangeDeltaMin).

can not find symbol info "nt_kernel_data.modules[0]->rom->recalib_config->MutRangeDeltaMax"

Symbol nt_kernel_data.modules[0]->rom->recalib_config->MutRangeDeltaMax not found.Symbol not found (nt_kernel_data.modules[0]->rom->recalib_config->MutRangeDeltaMax).

How can I solve this?

I have taken the folder located at C:\Users\user\AppData\Local\Temp\pcm1CB9.tmp, assuming this is the correct one?

0 Kudos
Reply

2,816 Views
iulian_stan
NXP Employee
NXP Employee

It generates a different temporary folder each time, so the content should be the same  in all pvmXYZ.tmp folders.

Judging by the error message, it fails to find some project symbols. Unfortunately I don't have the hardware setup to verify it (nor am I familiar with this project) so a quick guess - I'd try loading symbol file manually:

  1. Navigate to  Project→Options...→Map Files and select the your project binary file.
    Capture.PNG
  2.  Press the button next to Default symbol file input field and select the .afx file

    Capture.PNG

  3. Once it is loaded, FreeMASTER should extract symbolic information from debug section (you can see the parsed symbols by pressing the View button)Capture.PNG

Regards,

Iulian

0 Kudos
Reply