Data flow of S32K344 (RD-HVBMSCTBUN) Integration Project using FreeMASTER

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Data flow of S32K344 (RD-HVBMSCTBUN) Integration Project using FreeMASTER

1,297件の閲覧回数
Bearich
Contributor I

Hello, this is JJ

 

I'm using the RD-HVBMSCTBUN board kit.

I wonder the data flow from physical board to FreeMASTER in Integration project from package manager.

 

What is the function, variable, or method to read the VIT?

If I know the way to get voltage for example, current and temperature would be similar way.

and what is the function, variable, or method to send the VIT data to FreeMASTER?

 

Bearich_0-1716915067257.pngBearich_0-1716915067257.png

like this function in the HvBms_CmuSenseMon.c file, where the result flows from this function?

 

please let me know some clue,,

0 件の賞賛
返信
0 返答(返信)