Application Command issue in 'examples/freemaster_examples/fmstr_example_pdbdm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Application Command issue in 'examples/freemaster_examples/fmstr_example_pdbdm

Jump to solution
477 Views
pberna67
Contributor III

Dear All

Downloaded sdk.sdk_2.x_lpcxpresso54114 with only FreeMASTER examples. It works correctly in any aspect apart the Application Command section where I find strange behavior

More details has been posted in github here:

https://github.com/nxp-mcuxpresso/mcuxsdk-examples/issues/10


Regards

Paolo

 

0 Kudos
Reply
1 Solution
420 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello, if I understand the issue correctly, you do not see a reason why command 0x10 returns code 16 in the example application.

The command 0x10 is registered for a callback function:

MichalH_0-1790669419958.png

So the function "my_appcmd_handler" gets called automatically when FreeMASTER probes the command execution.  The example code of this callback is quite trivial:

MichalH_1-1790669515160.png

Which is the reason you get the return code 16 (=0x10) as answer.

I also confirm there is an issue in FreeMASTER with displaying a message for unknown responses as you reported for app.command with Id 0x02. The response 0xcd should be reported as "unknown response" but generates no message at all.

Thanks,
Michal

 

 

View solution in original post

0 Kudos
Reply
1 Reply
420 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello, if I understand the issue correctly, you do not see a reason why command 0x10 returns code 16 in the example application.

The command 0x10 is registered for a callback function:

MichalH_0-1790669419958.png

So the function "my_appcmd_handler" gets called automatically when FreeMASTER probes the command execution.  The example code of this callback is quite trivial:

MichalH_1-1790669515160.png

Which is the reason you get the return code 16 (=0x10) as answer.

I also confirm there is an issue in FreeMASTER with displaying a message for unknown responses as you reported for app.command with Id 0x02. The response 0xcd should be reported as "unknown response" but generates no message at all.

Thanks,
Michal

 

 

0 Kudos
Reply