FTF 2015 トレーニングプレゼンテーション

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FTF 2015 Training Presentations

ディスカッション

ソート順:
The Kinetis family of MCUs is in constant growth and has become the most scalable and wide MCU family in the market based on ARM® Cortex™-M processors. KinetisK series, ARM Cortex-M4 based, is adding new cost-effective devices and memory densities. The Kinetis L family, based on the ARM Cortex M0+ core, grows with more ultra-low power devices. The Kinetis W series offers wireless functionality by integrating class-leading sub-1 GHz and 2.4 GHz RF transceivers. For high accuracy electricity metering and test and measurement applications Kinetis M introduces 24-bit sigma delta ADC and low noise amplifiers on-chip. Kinetis V family offers new Motor Control possibilities starting with low cost ARM Cortex M0+ based devices. But there is more to come! This session offers an overview of the current status of Kinetis families and roadmaps.
記事全体を表示
The D-Bug12XZ firmware combined with the Freescale LFBDMPGMR BDM programmer hardware provides a powerful low-level debugging environment for S12 and S12X MagniV devices. There are times when Electronic Control Modules (ECM) in a car will become inoperative or unresponsive to normal communication channels such as CAN or LIN. The Background Debug Module (BDM) on these devices combined with the D-Bug12XZ  debugger provides the ability to reliably ‘hot-connect’ to the S12 and S12X MagniV devices without resetting or disturbing the running target. Once BDM communications is established with the target, the MCU’s I/O and memory resources can be uploaded for analysis. This session will teach the features and use of these tools to ‘hot connect’ to an unresponsive target MCU with the goal of determining the possible cause of the software and/or hardware failure.
記事全体を表示
This session will cover how to differentiate and to attach Freescale Power Management solutions to most Freescale MCU and MPUs for complete system enablement in IoT, automotive and multi-market applications. Thanks to a complete MCU tool alignment strategy for industrial applications in Transportation, Energy Management and Building Control segments, we can provide the fastest time to market for your customers. The presentation will include live demonstrations  with analog software drivers that are MCU agnostic, in order to better position Freescale Analog System solutions during your next customer visit.
記事全体を表示
How to develop a proper GUI with FreeMASTER and integrate it to a MCU for development and debugging purposes.
記事全体を表示
Freescale Connected Intelligence helps to bring the full potential of the IoT to life, delivering intelligence everywhere so designs and whole systems can scale and interact seamlessly and securely. This session will present the Freescale solutions addressing the challenges of IoT, with a focus on Wireless Connectivity platforms. Presented by Cyril Zarader Presented at DwF Tel Aviv - January 27, 2015 Session ID: EUF-IND-T0970
記事全体を表示
The Kinetis software development kit (SDK) provides a comprehensive software framework for Kinetis MCU-based applications. Join this session to get hands-on experience with the basics of Kinetis SDK, including MCU boot-up, board setup, interrupt handling, HAL and drivers.
記事全体を表示
This session will outline the design challenges that healthcare and medical device designers face when designing a product and selecting components. Special attention will be paid to IC selection, wireless connectivity, system security and regulatory concerns. Following this class, you should be better prepared to utilize Freescale products to get your products to market faster.
記事全体を表示
Introduction to functional safety at Freescale and understanding the generic fundamentals. This session will discuss the key content of the Safety Manual and Dynamic FMEDA, plus how they are used by the Automotive and Industrial customer.
記事全体を表示
How Freescale's RF device portfolio can solve problems for many different industries. The focus on uses outside of the traditional cellular infrastructure and how Freescale devices bring unique capabilities to these application areas that include: Industrial Scientific Medical (ISM) applications, including laser, MRI and heating; Land mobile, including public safety, dispatch and remote monitoring; Avionics, including communication, navigation and radar systems. Presented by Yan Vainter Presented at DwF Tel Aviv - January 27, 2015 Session ID: EUF-IND-T0977
記事全体を表示
In this hands-on workshop, learn how to build your next motor control application using Kinetis V series MCUs and Freescale’s comprehensive set of complimentary motor control software and tools, such as Freescale's Embedded Software Motor Control and Power Conversion Libraries (FSLESL), Kinetis SDK, Kinetis Design Studio IDE along with Tower System Module rapid prototyping - all designed specifically to reduce you development time.
記事全体を表示
Kinetis Microcontrollers (MCUs) consist of multiple hardware- and software-compatible ARM Cortex-M0+, Cortex-M4 and Cortex-M7-based MCU series. Kinetis MCUs offer exceptional low-power performance, scalability and feature integration.
記事全体を表示
PROFIBUS, CAN and RS232 are extensively used in communications networks in factories, buildings, transport infrastructures and monitoring/control equipment in our cities. Ethernet offers higher bandwidth and, in many cases, lowers cost--especially when deployed in daisy-chain topology. Technologies such as EtherCAT, PROFINET and EtherNet/IP are testament to this. In this session, we will explore how QorIQ processor families can help equipment manufacturers span this landscape using a QUICC Engine (QE) controller for UART/Ethernet-based protocol implementation, a Enhanced Triple Speed Ethernet Controller (eTSEC) for intelligent Ethernet classification and 2-port switching, and an eight-port gigabit Ethernet switch for wire-rate switching. Reference design software and hardware files will be available to help you start your own PROFIBUS and PROFINET designs. 
記事全体を表示
In this session, attendees will learn what types of applications can be built on a wearable reference platform for the healthcare and fitness markets. Design challenges and requirements for creating your own designs using WaRP, a wearable reference platform (WaRP), with Kinetis MCUs, i.MX applications processors and Freescale sensors will be discussed.
記事全体を表示
The QorIQ T1040 and T1042 communication processors support four integrated 64-bit e5500 Power Architecture® processor cores with high-performance data path acceleration architecture (DPAA) and network peripheral interfaces required for networking and telecommunications. This session will provide an in-depth look at the new features being introduced in the T1040 family such as the Single Source Clock, L2 Switch, sSDXC, QSGMII and DDR4. The session will also cover power-saving schemes of T1040. Presented by Du Chen​ Presented at DwF Digital Networking - Nanjing - 21 May 2015 Session ID: APF-SNT-T1359
記事全体を表示
Beginning 2016, the European New Car Assessment program (NCAP) will allocate increased scoring measures for pedestrian detection capabilities. This means that any car fitted with technologies that enable detection of a pedestrian in a hazardous situation and as a result perform collision avoidance measures shall be rewarded with an increased NCAP score. These systems must be designed and manufactured based on a solid automotive development flow. This session will address the vision processing requirements for pedestrian detection and provide training on how vision algorithms may be implemented to respond to NCAP requirements in a safe, secure and reliable way.
記事全体を表示
Some IoT installations are required to maintain operations in the field for over 10 years. Selecting sensor components for these applications is significantly different from mobile and consumer products. This presentation examines environmental compatibility and long term operating characteristics of sensors and provides an overview of the design considerations for embedded industrial applications.
記事全体を表示
Kinetis M series MCUs are based upon the low-power ARM® Cortex®-M0+ core and are designed for single-chip 1, 2 and 3-phase electricity meters as well as flow meter and other precision measurement applications.
記事全体を表示
High power RF customers also use low power MMICs and GPAs as smaller drivers and pre-driver which are included in Freescale's RF small signal portfolio. This class will cover the mathematics for computing the required driver and pre-driver output power in a line-up, discuss key product differentiators and review the small signal RF device portfolio. Since all radio communications systems include both a transmit path and a receive path, Freescale’s small signal portfolio contains an extensive array of low noise amplifier (LNA) devices used in the receive path of the radio link. This class will also cover the techniques used to create line-up suggestions utilizing these devices.
記事全体を表示
This session will discuss Advanced Driver Assistance Systems (ADAS) product and solution update plus feature guidelines on product mapping for different ADAS applications.
記事全体を表示