usb gadget mass-storage bugs in cdns-usb3 driver?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

usb gadget mass-storage bugs in cdns-usb3 driver?

824件の閲覧回数
Its_wen
Contributor I

root@imx8qxpc0mek:~# modprobe g_mass_storage file=test.img
[ 150.446776] Mass Storage Function, version: 2009/09/11
[ 150.451968] LUN: removable file: (no medium)
[ 150.456473] LUN: file: /home/root/test.img
[ 150.460612] Number of LUNs=1
[ 150.463741] g_mass_storage gadget.0: Mass Storage Gadget, version: 2009/09/11
[ 150.470932] g_mass_storage gadget.0: userspace failed to provide iSerialNumber
[ 150.478251] g_mass_storage gadget.0: g_mass_storage ready
root@imx8qxpc0mek:~# [ 151.193785] cdns-usb3 5b130000.usb: onchip mem is full, ep is invalid
[ 151.200317] cdns-usb3 5b130000.usb: onchip mem is full, ep is invalid
[ 151.206772] cdns-usb3 5b130000.usb: onchip mem is full, ep is invalid
[ 151.213334] cdns-usb3 5b130000.usb: timeout for waiting configuration set
[ 152.242820] g_mass_storage gadget.0: common->fsg is NULL in fsg_setup at 465
[ 152.249971] ------------[ cut here ]------------
[ 152.254593] WARNING: CPU: 0 PID: 180 at drivers/usb/gadget/function/f_mass_storage.c:314 __fsg_is_set.part.0.isra.0+0x24/0x38
[ 152.265930] Modules linked in: g_mass_storage fsl_jr_uio caam_jr snd_soc_imx_audmix caamkeyblob_desc caamhash_desc caamalg_desc crypto_engine authenc libdes crct10dif_ce polyval_ce polyval_generic snd_soce
[ 152.304557] CPU: 0 PID: 180 Comm: irq/448-5b13000 Tainted: G C 6.1.1+g29549c7073bf #1
[ 152.313789] Hardware name: Freescale i.MX8QXP MEK (DT)
[ 152.318933] pstate: 600000c5 (nZCv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 152.325906] pc : __fsg_is_set.part.0.isra.0+0x24/0x38
[ 152.330973] lr : __fsg_is_set.part.0.isra.0+0x24/0x38
[ 152.336035] sp : ffff80000adfbc00
[ 152.339354] x29: ffff80000adfbc00 x28: 0000000000000001 x27: ffff000811939810
[ 152.346512] x26: ffff000811939800 x25: ffff8000080ef250 x24: 0000000000000000
[ 152.353671] x23: 0000000000000000 x22: 0000000000000001 x21: ffff000817016400
[ 152.360829] x20: ffff0008101e8e00 x19: ffff80000a1ff000 x18: 0000000000000006
[ 152.367988] x17: 0000000000000000 x16: 0000000000000000 x15: ffff80000adfb680
[ 152.375146] x14: 0000000000000000 x13: ffff800009d32428 x12: 00000000000006c6
[ 152.382305] x11: 0000000000000242 x10: ffff800009d8a428 x9 : ffff800009d32428
[ 152.389463] x8 : 00000000ffffefff x7 : ffff800009d8a428 x6 : 80000000fffff000
[ 152.396622] x5 : ffff00083c9b2a18 x4 : ffff00083c9b2a18 x3 : 0000000000000000
[ 152.403780] x2 : 0000000000000000 x1 : 0000000000000000 x0 : ffff000811b749c0
[ 152.410942] Call trace:
[ 152.413392] __fsg_is_set.part.0.isra.0+0x24/0x38
[ 152.418117] fsg_setup+0x10c/0x1c0
[ 152.421529] composite_setup+0x468/0x17f4
[ 152.425562] cdns3_check_ep0_interrupt_proceed+0x284/0x5d0
[ 152.431059] cdns3_device_thread_irq_handler+0x508/0xa10
[ 152.436385] irq_thread_fn+0x2c/0xb0
[ 152.439973] irq_thread+0x16c/0x250
[ 152.443474] kthread+0x108/0x10c
[ 152.446716] ret_from_fork+0x10/0x20
[ 152.450305] ---[ end trace 0000000000000000 ]---
[ 173.597007] cdns-usb3 5b130000.usb: onchip mem is full, ep is invalid
[ 173.603539] cdns-usb3 5b130000.usb: onchip mem is full, ep is invalid
[ 173.609994] cdns-usb3 5b130000.usb: onchip mem is full, ep is invalid
[ 173.616554] cdns-usb3 5b130000.usb: timeout for waiting configuration set

root@imx8qxpc0mek:~# uname -r
6.1.1+g29549c7073bf

0 件の賞賛
返信
0 返答(返信)