ptp / enet driver problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ptp / enet driver problem

3,226件の閲覧回数
andylime
Contributor I

I am porting the AN12149 ptp application note to the most recent SDK.

There are a very big differences between the fsl_enet.c FSL_ENET_DRIVER_VERSION (MAKE_VERSION(2, 3, 0)) and FSL_ENET_DRIVER_VERSION (MAKE_VERSION(2, 2, 3)), there are literally missing a lot of ieee1588 functionality  like ENET_GetRxFrameTime just to mention one.

This makes it impossible to port the application.

It is somehow surprising that the library exist without being recently backwards compatible.

Do there exist any workaround to fix the incompatibility or an explanation  ?

Regards Andy 

0 件の賞賛
返信
2 返答(返信)

2,325件の閲覧回数
np
Contributor IV

I too am looking at these same missing functions. We had AN12149-based PTP working with a (much) older version of the SDK, but it's hard to know where to start without ENET_GetRxFrameTime() and ENET_GetTxFrameTime() to name but two, these are such low-level functions.

Or is PTP basically not supported any more?

0 件の賞賛
返信

3,081件の閲覧回数
xabiermarquiegu
Contributor II

Hello,

I'm interested in this code. Did you make any progress on this?

0 件の賞賛
返信