nnstreamer_python import error in postprocess_yolov4_tiny.py script

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

nnstreamer_python import error in postprocess_yolov4_tiny.py script

1,615 次查看
amrithkrish
Contributor I

Hi,

I'm trying to run a custom Yolov3 model on imx8MP using NNStreamer. I had followed the the documentation provided here - https://github.com/nxp-imx/nxp-nnstreamer-examples.git -> detection -> example_detection_yolo_v4_tiny_tflite.sh  for reshaping and post processing the output tensors so that it can be used by the tensor_decoder.

 

However the Python script called from the above shell script (available at : https://github.com/nxp-imx/nxp-nnstreamer-examples.git -> detection -> postprocess_yolov4_tiny.py ) uses a nnstreamer_python module.

I'm not able to find or install the same package to my system. Could you please help me with this?  

0 项奖励
回复
0 回复数