i.mx7 host cortex m4 cpu i2s driver example code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx7 host cortex m4 cpu i2s driver example code

1,342件の閲覧回数
mehmetrizaoz
Contributor I

Hello, 

I am using i.mx 7dual host for a medical device project. I am using m4 as a helper processor. I have to play some audio files through m4 via speakers. There isn't a specific decoder or container limitation for these ready to play audio files. We can choose/convert the format or use even some custom format without any compression. Is there an example code to use i2s peripheral on m4 core?

Thanks

 

タグ(1)
0 件の賞賛
返信
0 返答(返信)