eIQ ToolKit Remote Devices

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eIQ ToolKit Remote Devices

2,533 Views
HT_MOB
Contributor II

I want to validate a deep learning model on imx8mp.
I'm using the eIQ ToolKit.

I cannot add imx8mp from the Remote Devices tab.
"Validation Error: Could not find devices." Is displayed.

I want to solve this problem, but I don't know where to suspect the problem.

By the way, the device is connected to the PC with a LAN cable.
It is possible to connect to device with ssh from the command line of the PC.

1 Reply

1,919 Views
_asif_muhammed_
Contributor III

Were you able to resolve that issue? I am also facing the same issue.

 

0 Kudos
Reply