Using an External Antenna

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using an External Antenna

3,384件の閲覧回数
eortega
Contributor II

Hello!

From going through the docs, while we do not need to use an external antenna, if we did want to use an external antenna on the QN9080 DK board - all we would need to do is plug in the RF connector to the RF port and that would enable the switch to utilize the external antenna instead of the internal antenna?

If any one can clarify this that would be most helpful, thank you.

Eduardo

タグ(2)
0 件の賞賛
返信
2 返答(返信)

3,322件の閲覧回数
eortega
Contributor II

Replying to myself - the switch is a murata RF switch so by plugging in an RF connector we may be able to switch the signal from the MIFA internal antenna to the external antenna

0 件の賞賛
返信

3,322件の閲覧回数
eortega
Contributor II

Or if anyone knows a software method to lower signal strength through the built in antenna, please let me know!

Eduardo

0 件の賞賛
返信