Using Config Tools via MCUXpresso for VS code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using Config Tools via MCUXpresso for VS code

1,728 次查看
CktDesigner
Contributor IV

I converted a project from the MCUXpresso IDE to MCUXpresso for VS code.

The project is for a custom board that uses the MIMXRT1062CVL5B processor.

The project compiles using the MCUXpresso IDE.

I'm using MCUXpresso Config Tools Version 15.0

I'm using Visual Studio Code Version 1.90.2 with Version 1.9 of MCUXpresso for VS Code extension

After importing the project into VScode (and manually modifying a couple of things that didn't convert properly), it now compiles in VScode.

I configured the project pins and peripherals using the Config Tool in MCUXpresso IDE.

When I open the Config Tool via VScode, I get errors stating that some drivers are not found in the toolchain/IDE project. These errors don't show up when using the IDE version.

The drivers are there and the code compiles!

The Errors can be resolved by clicking Edit->Undo Custom toolchain project link (although the Information item "No toolchain project is detected" still shows up in the Problems tab!!

I then save the Configuration File (.mex). But if I close the Config Tool, then later re-open it, the same error exists.

Also, if I want to add a new component to the project, I can click on the Config Tool Peripheral driver tab and add the component, but the driver doesn't get added to the project. (This can be done when using the "IDE" version.) Is there a different procedure to do this in the "VS code" version?

Thanks!

0 项奖励
回复
0 回复数