Synchronous Abort handler

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Synchronous Abort handler

2,470 次查看
st_ra
Contributor II

Hi,

I load fsl-image-auto .sdcard file onto SDcard. Added u-boot.bin to uboot partition. Im using bootloader from platform software integration packet and loading u-boot to address 0x34090000 with reset handler address set to 0x340a0000. u-boot.bin successfully loads to RAM, and I can see it starts in console. But I get following error and board just resets and always same console output:

U-Boot 2020.04+g6286902c94 (Nov 17 2021 - 08:47:30 +0000)

CPU: NXP S32G274A rev. 2.1.0
Reset cause: Power-On Reset
Model: NXP S32G2XX
Board:  NXP S32G274A-RDB
DRAM:  3.5 GiB
"Synchronous Abort" handler, esr 0x96000010
elr: 00000000340d8f78 lr : 00000000340d8f64 (reloc)
elr: 00000000fff6ff78 lr : 00000000fff6ff64
x0 : 0000000000000001 x1 : 0000000000000042
x2 : 00000000ffffffff x3 : 0000000000000002
x4 : 00000000fff700f0 x5 : 00000000ffffffff
x6 : 0000000000000021 x7 : 0000000000000000
x8 : 00000000ffd34f40 x9 : 000000000000000c
x10: 00000000fff9b818 x11: 00000000ffd2d32c
x12: 0000000000002a80 x13: 00000000ffd2d38c
x14: 00000000ffd2d5b8 x15: 0000000000000001
x16: 00000000fff7c068 x17: 00000000000000ff
x18: 00000000ffd32dd8 x19: 0000000000000000
x20: 00000000fff9f9d4 x21: 0000000000000000
x22: 0000000000000002 x23: 0000000000000021
x24: 00000000ffd37e60 x25: 00000000fffa81a9
x26: 0000000000000042 x27: 0000000000000002
x28: 00000000402dc000 x29: 00000000ffd2d310

Code: b9407fe0 1ad52363 93407c76 340006e0 (387c6ac0)
Resetting CPU ...

resetting ...

Im using S32G274A RDB2 board. Linux BSP is v31.

0 项奖励
回复
1 回复

2,456 次查看
st_ra
Contributor II

Found problem, had to add I2C3 and I2C4 to xRDC peripherals for A53.

Now Im faced with new issue, M7 core running fine, but linux gets stuck here:

[    4.036637] Waiting for root device /dev/mmcblk0p2...
[   11.067250] mmc0: Timeout waiting for hardware cmd interrupt.
[   11.067258] mmc0: sdhci: ============ SDHCI REGISTER DUMP ===========
[   11.067264] mmc0: sdhci: Sys addr:  0x00000000 | Version:  0x00000002
[   11.067270] mmc0: sdhci: Blk size:  0x00000200 | Blk cnt:  0x00000001
[   11.067276] mmc0: sdhci: Argument:  0x00000c00 | Trn mode: 0x00000000
[   11.067282] mmc0: sdhci: Present:   0x01fd8009 | Host ctl: 0x00000001
[   11.067287] mmc0: sdhci: Power:     0x00000000 | Blk gap:  0x00000080
[   11.067292] mmc0: sdhci: Wake-up:   0x00000008 | Clock:    0x000020ff
[   11.067298] mmc0: sdhci: Timeout:   0x0000008c | Int stat: 0x00018000
[   11.067303] mmc0: sdhci: Int enab:  0x007f1003 | Sig enab: 0x007f1003
[   11.067308] mmc0: sdhci: ACmd stat: 0x00000000 | Slot int: 0x00000502
[   11.067314] mmc0: sdhci: Caps:      0x07eb0000 | Caps_1:   0x8000b407
[   11.067319] mmc0: sdhci: Cmd:       0x0000341a | Max curr: 0x00ffffff
[   11.067325] mmc0: sdhci: Resp[0]:   0x00000b00 | Resp[1]:  0x0073677f
[   11.067330] mmc0: sdhci: Resp[2]:   0x325b5900 | Resp[3]:  0x00400e00
[   11.067336] mmc0: sdhci: Host ctl2: 0x00000000
[   11.067340] mmc0: sdhci: ADMA Err:  0x00000000 | ADMA Ptr: 0x00000000
[   11.067345] mmc0: sdhci-esdhc-imx: ========= ESDHC IMX DEBUG STATUS DUMP =========
[   11.067350] mmc0: sdhci-esdhc-imx: cmd debug status:  0x2100
[   11.067355] mmc0: sdhci-esdhc-imx: data debug status:  0x2200
[   11.067360] mmc0: sdhci-esdhc-imx: trans debug status:  0x2300
[   11.067366] mmc0: sdhci-esdhc-imx: dma debug status:  0x2400
[   11.067372] mmc0: sdhci-esdhc-imx: adma debug status:  0x2500
[   11.067379] mmc0: sdhci-esdhc-imx: fifo debug status:  0x2680
[   11.067385] mmc0: sdhci-esdhc-imx: async fifo debug status:  0x2750
[   11.067391] mmc0: sdhci: ============================================

Any idea what could be problem? This does not happen when M7 application is not running.

0 项奖励
回复