Set HDMI resolution on linux in imx 8m plus evk board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Set HDMI resolution on linux in imx 8m plus evk board

618 Views
bych
Contributor II

I have imx 8m plus evk and flashed a image-full (version L6. 1.1_1.0.1) in the board.

After boot from emmc, the linux os works fine.

 

But after I connected HDMI cable to a 7-inch monitor I have, the pixel resolution doesn't seem to fit the entire screen which has pixels of 1024x600.

The Linux Screen shows only two-thirds of panel.

 

Can anyone help me to set HDMI pixel resolution to get a linux screen that fits to the panel of 1024x600 pixels?

 

0 Kudos
Reply
0 Replies