SB32 RDB2 support TEE? If yes, how can I activate TEE on RDB2?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SB32 RDB2 support TEE? If yes, how can I activate TEE on RDB2?

962 次查看
tylor
Contributor I

Hello, Team.

 

Is TEE(op-tee) supported on S32 RDB2 board?

I can not find the guidance or example for that.

And I just tried to set TZ memory address for the board but it shows me error message like below

 

NOTICE: BL2: v2.5(release):bsp33.0-2.5-dirty
NOTICE: BL2: Built : 14:01:09, Jun 15 2022
NOTICE: BL2: Booting BL31
E/TC:0 0 crypto_driver_init:369 Firmware not found
E/TC:0 0 call_initcalls:24 Initcall __text_start + 0x0005d200 failed

 

and op-tee client is pending when SESSION_OPEN when I used optee-examples or xtest?

Any Help?

0 项奖励
回复
0 回复数