S32K144: IAR SW issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K144: IAR SW issue

205 次查看
Alex28
Contributor I

Under IAR, debugging can still be done when the interrupt vector table is not at position 0. What are the specific principles and processes?

0 项奖励
回复
1 回复

134 次查看
yisey
Contributor I

Under IAR, debugging with the interrupt vector table not at position 0 works because the debugger uses the microcontroller’s vector relocation mechanism. The IVT can be remapped via a hardware register to a different memory address. IAR reads this relocation information at startup, maps interrupts to the relocated vectors, and monitors the memory region if the table is in RAM. When an interrupt occurs, the debugger traces execution from the relocated vector, allowing breakpoints, stepping through ISRs, and register monitoring as usual. When you need to Order Voice Talent Now, this ensures full debugging functionality even when the interrupt vectors are not at address 0.

0 项奖励
回复