P1020 NAND flash support, for a board which uses NOR flash for booting.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P1020 NAND flash support, for a board which uses NOR flash for booting.

872 次查看
johnclark
Contributor I

I am looking for information on either u-boot for the p1020 series, or for a linux driver which allows for use of a NAND flash device, in a situation were there is NOR flash used for standard booting processes.

When we implemented the board, we put both types of flash on the board, and now I have need to use the 256M NAND flash device.

Since the original board did not use the NAND flash the u-boot image does not contain any intitialization for it, and it appears that the linux driver does not get the correct OF device tree settings, to 'see' the device.

The current yucktoe package does not go that 'far back' in processors to support getting the current u-boot package and figuring this out.

0 项奖励
回复
0 回复数