Machine Learning i.MX RT1060

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Machine Learning i.MX RT1060

4,718件の閲覧回数
trsbalaji
Contributor I

Hi Team,

We will interested to learn Machine learning i.MX 1060. We will  get free hardware?

Because I got NXP imx6, NXP iMX7. Currently am not using because android things is stopped.

Thanks,

Balaji Babu

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

4,503件の閲覧回数
jc_pacheco
NXP Employee
NXP Employee

Hi Balaji,

The Software Clinic event offered a 20% discount (mentioned here) but no free boards were offered. This specific event focused on i.MXRT1050 and i.MXRT1060 crossover processors.

See below the current supported platforms and enablement. As you can see, Arm NN (v19.05) is fully integrated into Yocto recipe supporting i.MX 8 Series (eIQ officially supports the NXP i.MX 8 Series but it is possible to build eIQ for i.MX 6 and i.MX 7 Series).

pastedImage_1.png

Please refer to eIQ Software Fact Sheet and NXP eIQ Machine Learning Enablement for details about supported platforms, features and software available with NXP eIQ.

Regards,

JC

0 件の賞賛
返信

4,503件の閲覧回数
trsbalaji
Contributor I

Thanks Junan.

Could you please share the link how to build yocto image with machine learning.

Regards,

Balaji Babu

0 件の賞賛
返信

4,503件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信