LS1046 I2C for i2c3 cannot work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046 I2C for i2c3 cannot work

1,995 Views
Sally_Jay
Contributor I

I cannot scan the device on i2c-3

In dts,the configure is

i2c3: i2c@21b0000 {
compatible = "fsl,vf610-i2c", "fsl,ls1046a-vf610-i2c";
#address-cells = <1>;
#size-cells = <0>;
reg = <0x0 0x21b0000 0x0 0x10000>;
interrupts = <GIC_SPI 59 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clockgen 4 1>;
fsl-scl-gpio = <&gpio3 12 0>;
status = "okay";
};
 
I checked the datasheet
Sally_Jay_0-1757378211038.pngSally_Jay_1-1757378233845.png

from the datasheet,it says the default value is 0000_1111h.
I add the bellow command to rcw_1800_qspiboot_1133_5a59.rcw
.pbi
//SCFG_RCWPMUXCR0, configure IIC4_SCL/SDA=000
write 0x157040C, 0x00000000
.end
after I add above command, the device cannot boot up.
I tried 0x00000011, 0x00330000.
all values will cause the device cannot boot.
What value do i need to configure? or I need to do more configure for this function?

0 Kudos
Reply
1 Reply

1,155 Views
yisey
Contributor II

If you’re looking to redesign your living space, a virtual apartment designer can be a game-changer. It allows you to visualize furniture placement, color schemes, and decor before making any purchases. Using a virtual apartment designer helps save time, reduce costly mistakes, and experiment with different layouts easily. Many tools also offer realistic 3D renderings, making it easier to plan small or tricky spaces. Whether you’re moving into a new apartment or updating your current one, these tools make interior design more accessible and stress-free.

0 Kudos
Reply