K60 Swap feature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 Swap feature

1,273 Views
DrMurad
Contributor I

MK60FX512VLQ15

CodeWarrior

Section 30.4.12.14 of the Reference manual http://studio.segger.com/packages/Kinetis_K60/CMSIS/Documents/K60P144M150SF3RM.pdf

suggest that swap control is only available with "Program flash only devices).

if this is true, why are they refering to FlexNVM in FCCOB 6"

Our device has FlexNVM

Can we use the Swap feature?

how many Blocks in the Flash/Flex (logical, physical)?

if swap works, how can we use it with firmware size of 300 KB?

 

Regards,

Dr. Murad

0 Kudos
Reply
0 Replies