K60 Swap feature

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60 Swap feature

1,269件の閲覧回数
DrMurad
Contributor I

MK60FX512VLQ15

CodeWarrior

Section 30.4.12.14 of the Reference manual http://studio.segger.com/packages/Kinetis_K60/CMSIS/Documents/K60P144M150SF3RM.pdf

suggest that swap control is only available with "Program flash only devices).

if this is true, why are they refering to FlexNVM in FCCOB 6"

Our device has FlexNVM

Can we use the Swap feature?

how many Blocks in the Flash/Flex (logical, physical)?

if swap works, how can we use it with firmware size of 300 KB?

 

Regards,

Dr. Murad

0 件の賞賛
返信
0 返答(返信)