I.MX6DP: rootfs is not mounted at over linux-kernel 4.17 version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6DP: rootfs is not mounted at over linux-kernel 4.17 version

1,121 Views
AryzLee
Contributor I

Hello,

 

I use MFGTOOL2.0 to burn rootfs because UUU FBK has not worked well.

I have some difficult at mounting the rootfs. 

My custom board is consisted of I.MX6DP, nand, eMMC(for rootfs), DDR3, etc.

rootfs works well at the version of linux-kernel 4.16 below. but it doesn't work at over linux-kernel 4.17 r1 version.

It is related at MFGTOOL2.0 or UUU? Let me know your idea... 

the log as below.

======================================================================

1. 4.16 version is OKAY

[Mon Oct 16 09:30:30.351 2023] U-Boot 2023.07-00800-g247aa5a191-dirty (Oct 13 2023 - 11:49:24 +0900)
[Mon Oct 16 09:30:30.351 2023]
[Mon Oct 16 09:30:30.351 2023] CPU: Freescale i.MX6DP rev1.1 996 MHz (running at 792 MHz)
[Mon Oct 16 09:30:30.351 2023] CPU: Automotive temperature grade (-40C to 125C) at 35C
[Mon Oct 16 09:30:30.351 2023] Reset cause: POR
[Mon Oct 16 09:30:30.351 2023] Model: Freescale i.MX6 DualPlus Board
[Mon Oct 16 09:30:30.351 2023] Board: MX6Q-Sabreauto rev@
[Mon Oct 16 09:30:30.351 2023] DRAM: 1 GiB
[Mon Oct 16 09:30:30.399 2023] SETUP SPI...
[Mon Oct 16 09:30:31.428 2023] Core: 65 devices, 15 uclasses, devicetree: separate
[Mon Oct 16 09:30:31.428 2023] PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x21
[Mon Oct 16 09:30:31.428 2023] Flash: ## Unknown flash on Bank 1 - Size = 0x00000000 = 0 MB
[Mon Oct 16 09:30:31.428 2023] 0 Bytes
[Mon Oct 16 09:30:31.428 2023] NAND: 1024 MiB
[Mon Oct 16 09:30:31.444 2023] MMC:eMMC board_emmc_init...
[Mon Oct 16 09:30:31.464 2023] cfg->b_max:65535 cfg->f_min:400000 cfg->f_max:52000000
[Mon Oct 16 09:30:31.464 2023] FSL_SDHC: 0
[Mon Oct 16 09:30:31.464 2023] Loading Environment from MMC... at the mmc_startup
[Mon Oct 16 09:30:31.608 2023] *** Warning - bad CRC, using default environment
[Mon Oct 16 09:30:31.608 2023]
[Mon Oct 16 09:30:31.608 2023] Loading Environment from nowhere... OK
[Mon Oct 16 09:30:31.608 2023] In: serial@02020000
[Mon Oct 16 09:30:31.608 2023] Out: serial@02020000
[Mon Oct 16 09:30:31.608 2023] Err: serial@02020000
[Mon Oct 16 09:30:31.720 2023] SEC0: RNG instantiated
[Mon Oct 16 09:30:31.852 2023] switch to partitions #0, OK
[Mon Oct 16 09:30:31.852 2023] mmc0(part 0) is current device
[Mon Oct 16 09:30:31.852 2023] Net: eth0: ethernet@2188000 [PRIME]
[Mon Oct 16 09:30:31.960 2023] Hit any key to stop autoboot: 1 0
[Mon Oct 16 09:30:31.960 2023] STU iMX6 # setenv console "ttymxc0,115200"
[Mon Oct 16 09:30:36.553 2023] STU iMX6 # setenv bootargs "console=${console} root=/dev/mmcblk0p2 rootwait rw"
[Mon Oct 16 09:30:40.179 2023] STU iMX6 # setenv bootcmd "run bootargs; bootz ${loadaddr} - ${fdt_addr}"
[Mon Oct 16 09:30:43.785 2023] STU iMX6 # run bootcmd
[Mon Oct 16 09:30:46.828 2023] Unknown command 'rootwait' - try 'help'
[Mon Oct 16 09:30:46.828 2023] Kernel image @ 0x12000000 [ 0x000000 - 0x705d18 ]
[Mon Oct 16 09:30:46.828 2023] ## Flattened Device Tree blob at 18000000
[Mon Oct 16 09:30:46.828 2023] Booting using the fdt blob at 0x18000000
[Mon Oct 16 09:30:46.828 2023] Working FDT set to 18000000
[Mon Oct 16 09:30:46.828 2023] Using Device Tree in place at 18000000, end 1800a6a7
[Mon Oct 16 09:30:46.828 2023] Working FDT set to 18000000
[Mon Oct 16 09:30:46.828 2023]
[Mon Oct 16 09:30:46.828 2023] Starting kernel ...
[Mon Oct 16 09:30:46.828 2023]
[Mon Oct 16 09:30:47.547 2023] [ 0.000000] Booting Linux on physical CPU 0x0
[Mon Oct 16 09:30:47.911 2023] [ 0.000000] Linux version 4.16.0 (aryz@ubuntu) (gcc version 11.3.0 (GCC)) #1 SMP Mon Oct 16 08:59:44 KST 2023
[Mon Oct 16 09:30:47.911 2023] [ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d
[Mon Oct 16 09:30:47.911 2023] [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[Mon Oct 16 09:30:47.911 2023] [ 0.000000] OF: fdt: Machine model: Freescale i.MX6 DualPlus Board
[Mon Oct 16 09:30:47.911 2023] [ 0.000000] Memory policy: Data cache writealloc
[Mon Oct 16 09:30:47.911 2023] [ 0.000000] Reserved memory: created CMA memory pool at 0x3c000000, size 320 MiB
[Mon Oct 16 09:30:47.911 2023] [ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[Mon Oct 16 09:30:47.911 2023] [ 0.000000] random: get_random_bytes called from start_kernel+0x8c/0x40c with crng_init=0
[Mon Oct 16 09:30:47.911 2023] [ 0.000000] percpu: Embedded 16 pages/cpu @(ptrval) s36136 r8192 d21208 u65536
[Mon Oct 16 09:30:47.911 2023] [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 260608
[Mon Oct 16 09:30:47.911 2023] [ 0.000000] Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait rw
[Mon Oct 16 09:30:47.911 2023] [ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[Mon Oct 16 09:30:47.927 2023] [ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[Mon Oct 16 09:30:47.927 2023] [ 0.000000] Memory: 687960K/1048576K available (10240K kernel code, 493K rwdata, 3076K rodata, 1024K init, 7710K bss, 32936K reserved, 327680K cma-reserved, 0K highmem)
[Mon Oct 16 09:30:47.927 2023] [ 0.000000] Virtual kernel memory layout:
[Mon Oct 16 09:30:47.927 2023] [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[Mon Oct 16 09:30:47.927 2023] [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[Mon Oct 16 09:30:47.927 2023] [ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[Mon Oct 16 09:30:47.927 2023] [ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[Mon Oct 16 09:30:47.927 2023] [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[Mon Oct 16 09:30:47.927 2023] [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[Mon Oct 16 09:30:47.927 2023] [ 0.000000] .text : 0x(ptrval) - 0x(ptrval) (11232 kB)
[Mon Oct 16 09:30:47.927 2023] [ 0.000000] .init : 0x(ptrval) - 0x(ptrval) (1024 kB)
[Mon Oct 16 09:30:47.927 2023] [ 0.000000] .data : 0x(ptrval) - 0x(ptrval) ( 494 kB)
[Mon Oct 16 09:30:47.927 2023] [ 0.000000] .bss : 0x(ptrval) - 0x(ptrval) (7711 kB)
[Mon Oct 16 09:30:47.927 2023] [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[Mon Oct 16 09:30:47.944 2023] [ 0.000000] Running RCU self tests
[Mon Oct 16 09:30:47.944 2023] [ 0.000000] Hierarchical RCU implementation.
[Mon Oct 16 09:30:47.944 2023] [ 0.000000] RCU event tracing is enabled.
[Mon Oct 16 09:30:47.944 2023] [ 0.000000] RCU lockdep checking is enabled.
[Mon Oct 16 09:30:47.944 2023] [ 0.000000] RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
[Mon Oct 16 09:30:47.944 2023] [ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[Mon Oct 16 09:30:47.944 2023] [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[Mon Oct 16 09:30:47.944 2023] [ 0.000000] L2C-310 erratum 769419 enabled
[Mon Oct 16 09:30:47.944 2023] [ 0.000000] L2C-310 enabling early BRESP for Cortex-A9
[Mon Oct 16 09:30:47.944 2023] [ 0.000000] L2C-310 full line of zeros enabled for Cortex-A9
[Mon Oct 16 09:30:47.944 2023] [ 0.000000] L2C-310 ID prefetch enabled, offset 16 lines
[Mon Oct 16 09:30:47.944 2023] [ 0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled
[Mon Oct 16 09:30:47.944 2023] [ 0.000000] L2C-310 cache controller enabled, 16 ways, 1024 kB
[Mon Oct 16 09:30:47.944 2023] [ 0.000000] L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76470001
[Mon Oct 16 09:30:47.944 2023] [ 0.000000] Switching to timer-based delay loop, resolution 15ns
[Mon Oct 16 09:30:47.944 2023] [ 0.000008] sched_clock: 32 bits at 66MHz, resolution 15ns, wraps every 32537631224ns
[Mon Oct 16 09:30:47.952 2023] [ 0.000032] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 28958491609 ns
[Mon Oct 16 09:30:47.952 2023] [ 0.001068] Console: colour dummy device 80x30
[Mon Oct 16 09:30:47.952 2023] [ 0.001097] Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar
[Mon Oct 16 09:30:47.952 2023] [ 0.001114] ... MAX_LOCKDEP_SUBCLASSES: 8
[Mon Oct 16 09:30:47.952 2023] [ 0.001130] ... MAX_LOCK_DEPTH: 48
[Mon Oct 16 09:30:47.952 2023] [ 0.001146] ... MAX_LOCKDEP_KEYS: 8191
[Mon Oct 16 09:30:47.952 2023] [ 0.001161] ... CLASSHASH_SIZE: 4096
[Mon Oct 16 09:30:47.952 2023] [ 0.001177] ... MAX_LOCKDEP_ENTRIES: 32768
[Mon Oct 16 09:30:47.952 2023] [ 0.001191] ... MAX_LOCKDEP_CHAINS: 65536
[Mon Oct 16 09:30:47.952 2023] [ 0.001206] ... CHAINHASH_SIZE: 32768
[Mon Oct 16 09:30:47.952 2023] [ 0.001221] memory used by lock dependency info: 4655 kB
[Mon Oct 16 09:30:47.952 2023] [ 0.001238] per task-struct memory footprint: 1536 bytes
[Mon Oct 16 09:30:47.952 2023] [ 0.001287] Calibrating delay loop (skipped), value calculated using timer frequency.. 132.00 BogoMIPS (lpj=660000)
[Mon Oct 16 09:30:47.952 2023] [ 0.001319] pid_max: default: 32768 minimum: 301
[Mon Oct 16 09:30:48.256 2023] [ 0.001626] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[Mon Oct 16 09:30:48.256 2023] [ 0.001662] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[Mon Oct 16 09:30:48.256 2023] [ 0.003198] CPU: Testing write buffer coherency: ok
[Mon Oct 16 09:30:48.256 2023] [ 0.003981] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[Mon Oct 16 09:30:48.256 2023] [ 0.005133] Setting up static identity map for 0x10100000 - 0x10100078
[Mon Oct 16 09:30:48.256 2023] [ 0.005541] Hierarchical SRCU implementation.
[Mon Oct 16 09:30:48.256 2023] [ 0.007008] smp: Bringing up secondary CPUs ...
[Mon Oct 16 09:30:48.256 2023] [ 0.008727] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[Mon Oct 16 09:30:48.256 2023] [ 0.009269] smp: Brought up 1 node, 2 CPUs
[Mon Oct 16 09:30:48.256 2023] [ 0.009303] SMP: Total of 2 processors activated (264.00 BogoMIPS).
[Mon Oct 16 09:30:48.256 2023] [ 0.009321] CPU: All CPU(s) started in SVC mode.
[Mon Oct 16 09:30:48.256 2023] [ 0.011417] devtmpfs: initialized
[Mon Oct 16 09:30:48.256 2023] [ 0.025903] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[Mon Oct 16 09:30:48.256 2023] [ 0.027712] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[Mon Oct 16 09:30:48.256 2023] [ 0.027755] futex hash table entries: 512 (order: 3, 32768 bytes)
[Mon Oct 16 09:30:48.256 2023] [ 0.031696] cma: CMA area linux,cma could not be activated
[Mon Oct 16 09:30:48.272 2023] [ 0.031908] pinctrl core: initialized pinctrl subsystem
[Mon Oct 16 09:30:48.272 2023] [ 0.034956] NET: Registered protocol family 16
[Mon Oct 16 09:30:48.272 2023] [ 0.035264] DMA: failed to allocate 256 KiB pool for atomic coherent allocation
[Mon Oct 16 09:30:48.272 2023] [ 0.037648] cpuidle: using governor menu
[Mon Oct 16 09:30:48.272 2023] [ 0.037797] CPU identified as i.MX6Q, silicon rev 1.1
[Mon Oct 16 09:30:48.272 2023] [ 0.048292] vdd1p1: supplied by regulator-dummy
[Mon Oct 16 09:30:48.272 2023] [ 0.049441] vdd3p0: supplied by regulator-dummy
[Mon Oct 16 09:30:48.272 2023] [ 0.050580] vdd2p5: supplied by regulator-dummy
[Mon Oct 16 09:30:48.272 2023] [ 0.051647] vddarm: supplied by regulator-dummy
[Mon Oct 16 09:30:48.272 2023] [ 0.052666] vddpu: supplied by regulator-dummy
[Mon Oct 16 09:30:48.272 2023] [ 0.060681] vddsoc: supplied by regulator-dummy
[Mon Oct 16 09:30:48.272 2023] [ 0.072944] No ATAGs?
[Mon Oct 16 09:30:48.272 2023] [ 0.073182] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[Mon Oct 16 09:30:48.272 2023] [ 0.073250] hw-breakpoint: maximum watchpoint size is 4 bytes.
[Mon Oct 16 09:30:48.272 2023] [ 0.075415] imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[Mon Oct 16 09:30:48.272 2023] [ 0.124430] mxs-dma 110000.dma-apbh: initialized
[Mon Oct 16 09:30:48.272 2023] [ 0.127020] vgaarb: loaded
[Mon Oct 16 09:30:48.286 2023] [ 0.127917] SCSI subsystem initialized
[Mon Oct 16 09:30:48.286 2023] [ 0.128936] usbcore: registered new interface driver usbfs
[Mon Oct 16 09:30:48.286 2023] [ 0.129100] usbcore: registered new interface driver hub
[Mon Oct 16 09:30:48.286 2023] [ 0.129299] usbcore: registered new device driver usb
[Mon Oct 16 09:30:48.286 2023] [ 0.132125] i2c i2c-0: IMX I2C adapter registered
[Mon Oct 16 09:30:48.286 2023] [ 0.132169] i2c i2c-0: can't use DMA, using PIO instead.
[Mon Oct 16 09:30:48.286 2023] [ 0.133483] i2c i2c-1: IMX I2C adapter registered
[Mon Oct 16 09:30:48.286 2023] [ 0.133520] i2c i2c-1: can't use DMA, using PIO instead.
[Mon Oct 16 09:30:48.286 2023] [ 0.134754] i2c i2c-2: IMX I2C adapter registered
[Mon Oct 16 09:30:48.286 2023] [ 0.134791] i2c i2c-2: can't use DMA, using PIO instead.
[Mon Oct 16 09:30:48.286 2023] [ 0.135001] media: Linux media interface: v0.10
[Mon Oct 16 09:30:48.286 2023] [ 0.135105] Linux video capture interface: v2.00
[Mon Oct 16 09:30:48.286 2023] [ 0.135470] pps_core: LinuxPPS API ver. 1 registered
[Mon Oct 16 09:30:48.286 2023] [ 0.135493] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[Mon Oct 16 09:30:48.286 2023] [ 0.135542] PTP clock support registered
[Mon Oct 16 09:30:48.286 2023] [ 0.136216] Advanced Linux Sound Architecture Driver Initialized.
[Mon Oct 16 09:30:48.286 2023] [ 0.138068] Bluetooth: Core ver 2.22
[Mon Oct 16 09:30:48.286 2023] [ 0.138164] NET: Registered protocol family 31
[Mon Oct 16 09:30:48.294 2023] [ 0.138185] Bluetooth: HCI device and connection manager initialized
[Mon Oct 16 09:30:48.294 2023] [ 0.138256] Bluetooth: HCI socket layer initialized
[Mon Oct 16 09:30:48.294 2023] [ 0.138287] Bluetooth: L2CAP socket layer initialized
[Mon Oct 16 09:30:48.294 2023] [ 0.138430] Bluetooth: SCO socket layer initialized
[Mon Oct 16 09:30:48.294 2023] [ 0.139817] clocksource: Switched to clocksource mxc_timer1
[Mon Oct 16 09:30:48.294 2023] [ 0.140399] VFS: Disk quotas dquot_6.6.0
[Mon Oct 16 09:30:48.294 2023] [ 0.140539] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[Mon Oct 16 09:30:48.294 2023] [ 0.164495] NET: Registered protocol family 2
[Mon Oct 16 09:30:48.294 2023] [ 0.166065] tcp_listen_portaddr_hash hash table entries: 512 (order: 2, 20480 bytes)
[Mon Oct 16 09:30:48.294 2023] [ 0.166276] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[Mon Oct 16 09:30:48.294 2023] [ 0.166422] TCP bind hash table entries: 8192 (order: 6, 294912 bytes)
[Mon Oct 16 09:30:48.294 2023] [ 0.169051] TCP: Hash tables configured (established 8192 bind 8192)
[Mon Oct 16 09:30:48.294 2023] [ 0.169487] UDP hash table entries: 512 (order: 3, 40960 bytes)
[Mon Oct 16 09:30:48.294 2023] [ 0.169994] UDP-Lite hash table entries: 512 (order: 3, 40960 bytes)
[Mon Oct 16 09:30:48.441 2023] [ 0.171009] NET: Registered protocol family 1
[Mon Oct 16 09:30:48.441 2023] [ 0.172574] RPC: Registered named UNIX socket transport module.
[Mon Oct 16 09:30:48.441 2023] [ 0.172620] RPC: Registered udp transport module.
[Mon Oct 16 09:30:48.441 2023] [ 0.172641] RPC: Registered tcp transport module.
[Mon Oct 16 09:30:48.441 2023] [ 0.172661] RPC: Registered tcp NFSv4.1 backchannel transport module.
[Mon Oct 16 09:30:48.441 2023] [ 0.175041] hw perfevents: no interrupt-affinity property for /soc/pmu, guessing.
[Mon Oct 16 09:30:48.441 2023] [ 0.175519] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
[Mon Oct 16 09:30:48.441 2023] [ 0.178775] Initialise system trusted keyrings
[Mon Oct 16 09:30:48.441 2023] [ 0.179270] workingset: timestamp_bits=30 max_order=18 bucket_order=0
[Mon Oct 16 09:30:48.441 2023] [ 0.193725] NFS: Registering the id_resolver key type
[Mon Oct 16 09:30:48.441 2023] [ 0.193820] Key type id_resolver registered
[Mon Oct 16 09:30:48.441 2023] [ 0.193866] Key type id_legacy registered
[Mon Oct 16 09:30:48.441 2023] [ 0.194002] jffs2: version 2.2. (NAND) ⓒ 2001-2006 Red Hat, Inc.
[Mon Oct 16 09:30:48.441 2023] [ 0.195322] fuse init (API version 7.26)
[Mon Oct 16 09:30:48.441 2023] [ 0.196726] random: fast init done
[Mon Oct 16 09:30:48.441 2023] [ 0.205381] Key type asymmetric registered
[Mon Oct 16 09:30:48.441 2023] [ 0.205489] Asymmetric key parser 'x509' registered
[Mon Oct 16 09:30:48.452 2023] [ 0.205666] bounce: pool size: 64 pages
[Mon Oct 16 09:30:48.452 2023] [ 0.205759] io scheduler noop registered
[Mon Oct 16 09:30:48.452 2023] [ 0.205782] io scheduler deadline registered
[Mon Oct 16 09:30:48.452 2023] [ 0.206088] io scheduler cfq registered (default)
[Mon Oct 16 09:30:48.452 2023] [ 0.206113] io scheduler mq-deadline registered
[Mon Oct 16 09:30:48.452 2023] [ 0.206133] io scheduler kyber registered
[Mon Oct 16 09:30:48.452 2023] [ 0.211558] imx-sdma 20ec000.sdma: initialisation failed with -12
[Mon Oct 16 09:30:48.452 2023] [ 0.211759] imx-sdma: probe of 20ec000.sdma failed with error -12
[Mon Oct 16 09:30:48.452 2023] [ 0.212868] imx-gpc 20dc000.gpc: more than 6 clocks
[Mon Oct 16 09:30:48.452 2023] [ 0.213576] imx-gpc: probe of 20dc000.gpc failed with error -22
[Mon Oct 16 09:30:48.452 2023] [ 0.216626] pfuze100-regulator 0-0008: Full layer: 2, Metal layer: 1
[Mon Oct 16 09:30:48.452 2023] [ 0.217471] pfuze100-regulator 0-0008: FAB: 0, FIN: 0
[Mon Oct 16 09:30:48.452 2023] [ 0.217495] pfuze100-regulator 0-0008: pfuze100 found.
[Mon Oct 16 09:30:48.452 2023] [ 0.241120] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 22, base_baud = 5000000) is a IMX
[Mon Oct 16 09:30:48.452 2023] [ 1.103325] console [ttymxc0] enabled
[Mon Oct 16 09:30:48.452 2023] [ 1.135628] brd: module loaded
[Mon Oct 16 09:30:48.474 2023] [ 1.161015] loop: module loaded
[Mon Oct 16 09:30:48.474 2023] [ 1.166844] at24 0-0050: 131072 byte 24c1024 EEPROM, writable, 1 bytes/write
[Mon Oct 16 09:30:48.535 2023] [ 1.178215] gpmi-nand 112000.gpmi-nand: Failed to request DMA channel.
[Mon Oct 16 09:30:48.535 2023] [ 1.184951] gpmi-nand: probe of 112000.gpmi-nand failed with error -22
[Mon Oct 16 09:30:48.535 2023] [ 1.194798] libphy: Fixed MDIO Bus: probed
[Mon Oct 16 09:30:48.535 2023] [ 1.200052] CAN device driver interface
[Mon Oct 16 09:30:48.535 2023] [ 1.207702] fec 2188000.ethernet: 2188000.ethernet supply phy not found, using dummy regulator
[Mon Oct 16 09:30:48.730 2023] [ 1.331109] pps pps0: new PPS source ptp0
[Mon Oct 16 09:30:48.730 2023] [ 1.337964] fec: probe of 2188000.ethernet failed with error -12
[Mon Oct 16 09:30:48.730 2023] [ 1.344993] usbcore: registered new interface driver asix
[Mon Oct 16 09:30:48.730 2023] [ 1.350552] usbcore: registered new interface driver ax88179_178a
[Mon Oct 16 09:30:48.730 2023] [ 1.356742] usbcore: registered new interface driver cdc_ether
[Mon Oct 16 09:30:48.730 2023] [ 1.362717] usbcore: registered new interface driver net1080
[Mon Oct 16 09:30:48.730 2023] [ 1.368471] usbcore: registered new interface driver cdc_subset
[Mon Oct 16 09:30:48.730 2023] [ 1.374528] usbcore: registered new interface driver zaurus
[Mon Oct 16 09:30:48.730 2023] [ 1.380280] usbcore: registered new interface driver cdc_ncm
[Mon Oct 16 09:30:48.730 2023] [ 1.385963] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[Mon Oct 16 09:30:48.730 2023] [ 1.392550] ehci-pci: EHCI PCI platform driver
[Mon Oct 16 09:30:48.730 2023] [ 1.397098] ehci-mxc: Freescale On-Chip EHCI Host driver
[Mon Oct 16 09:30:48.730 2023] [ 1.403016] usbcore: registered new interface driver usb-storage
[Mon Oct 16 09:30:48.730 2023] [ 1.420196] rtc-ds1307 2-0068: registered as rtc0
[Mon Oct 16 09:30:48.864 2023] [ 1.426508] i2c /dev entries driver
[Mon Oct 16 09:30:48.864 2023] [ 1.431954] IR NEC protocol handler initialized
[Mon Oct 16 09:30:48.864 2023] [ 1.436514] IR RC5(x/sz) protocol handler initialized
[Mon Oct 16 09:30:48.864 2023] [ 1.441656] IR RC6 protocol handler initialized
[Mon Oct 16 09:30:48.864 2023] [ 1.446212] IR JVC protocol handler initialized
[Mon Oct 16 09:30:48.864 2023] [ 1.450841] IR Sony protocol handler initialized
[Mon Oct 16 09:30:48.864 2023] [ 1.455482] IR SANYO protocol handler initialized
[Mon Oct 16 09:30:48.864 2023] [ 1.460255] IR Sharp protocol handler initialized
[Mon Oct 16 09:30:48.864 2023] [ 1.464983] IR MCE Keyboard/mouse protocol handler initialized
[Mon Oct 16 09:30:48.864 2023] [ 1.470879] IR XMP protocol handler initialized
[Mon Oct 16 09:30:48.864 2023] [ 1.479198] imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
[Mon Oct 16 09:30:48.864 2023] [ 1.485350] Bluetooth: HCI UART driver ver 2.3
[Mon Oct 16 09:30:48.864 2023] [ 1.489876] Bluetooth: HCI UART protocol H4 registered
[Mon Oct 16 09:30:48.864 2023] [ 1.495367] Bluetooth: HCI UART protocol LL registered
[Mon Oct 16 09:30:48.864 2023] [ 1.501399] sdhci: Secure Digital Host Controller Interface driver
[Mon Oct 16 09:30:48.864 2023] [ 1.507603] sdhci: Copyright(c) Pierre Ossman
[Mon Oct 16 09:30:48.864 2023] [ 1.512032] sdhci-pltfm: SDHCI platform and OF driver helper
[Mon Oct 16 09:30:48.864 2023] [ 1.519230] mmc0: Unable to allocate ADMA buffers - falling back to standard DMA
[Mon Oct 16 09:30:48.868 2023] [ 1.526845] mmc0 bounce up to 128 segments into one, max segment size 65536 bytes
[Mon Oct 16 09:30:48.927 2023] [ 1.568897] mmc0: SDHCI controller on 2198000.usdhc [2198000.usdhc] using DMA
[Mon Oct 16 09:30:48.927 2023] [ 1.582300] caam 2100000.crypto: device ID = 0x0a16010000000000 (Era -524)
[Mon Oct 16 09:30:48.927 2023] [ 1.589241] caam 2100000.crypto: job rings = 2, qi = 0, dpaa2 = no
[Mon Oct 16 09:30:48.927 2023] [ 1.597964] caam_jr: probe of 2101000.jr failed with error -12
[Mon Oct 16 09:30:48.927 2023] [ 1.604612] caam_jr: probe of 2102000.jr failed with error -12
[Mon Oct 16 09:30:48.967 2023] [ 1.625699] caam algorithms registered in /proc/crypto
[Mon Oct 16 09:30:48.967 2023] [ 1.633573] Job Ring Device allocation for transform failed
[Mon Oct 16 09:30:48.967 2023] [ 1.640207] usbcore: registered new interface driver usbhid
[Mon Oct 16 09:30:48.967 2023] [ 1.645838] usbhid: USB HID core driver
[Mon Oct 16 09:30:49.094 2023] [ 1.662472] NET: Registered protocol family 10
[Mon Oct 16 09:30:49.094 2023] [ 1.671428] Segment Routing with IPv6
[Mon Oct 16 09:30:49.094 2023] [ 1.675332] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[Mon Oct 16 09:30:49.094 2023] [ 1.676361] mmc0: Switching to 1.8V signalling voltage failed
[Mon Oct 16 09:30:49.094 2023] [ 1.682920] NET: Registered protocol family 17
[Mon Oct 16 09:30:49.094 2023] [ 1.691726] can: controller area network core (rev 20170425 abi 9)
[Mon Oct 16 09:30:49.094 2023] [ 1.692978] mmc0: new DDR MMC card at address 0001
[Mon Oct 16 09:30:49.094 2023] [ 1.698088] NET: Registered protocol family 29
[Mon Oct 16 09:30:49.094 2023] [ 1.705351] mmcblk0: mmc0:0001 G1M15L 29.6 GiB
[Mon Oct 16 09:30:49.094 2023] [ 1.707329] can: raw protocol (rev 20170425)
[Mon Oct 16 09:30:49.094 2023] [ 1.713440] mmcblk0boot0: mmc0:0001 G1M15L partition 1 31.5 MiB
[Mon Oct 16 09:30:49.094 2023] [ 1.716429] can: broadcast manager protocol (rev 20170425 t)
[Mon Oct 16 09:30:49.094 2023] [ 1.723830] mmcblk0boot1: mmc0:0001 G1M15L partition 2 31.5 MiB
[Mon Oct 16 09:30:49.094 2023] [ 1.728077] can: netlink gateway (rev 20170425) max_hops=1
[Mon Oct 16 09:30:49.094 2023] [ 1.740014] mmcblk0rpmb: mmc0:0001 G1M15L partition 3 4.00 MiB, chardev (245:0)
[Mon Oct 16 09:30:49.094 2023] [ 1.740357] Key type dns_resolver registered
[Mon Oct 16 09:30:49.094 2023] [ 1.755626] Registering SWP/SWPB emulation handler
[Mon Oct 16 09:30:49.094 2023] [ 1.762931] Loading compiled-in X.509 certificates
[Mon Oct 16 09:30:49.100 2023] [ 1.768374] mmcblk0: p1 p2
[Mon Oct 16 09:30:49.212 2023] [ 1.818282] imx_thermal 20c8000.anatop:tempmon: Automotive CPU temperature grade - max:125C critical:120C passive:115C
[Mon Oct 16 09:30:49.212 2023] [ 1.834141] rtc-ds1307 2-0068: setting system clock to 2023-03-03 10:01:29 UTC (1677837689)
[Mon Oct 16 09:30:49.212 2023] [ 1.842850] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[Mon Oct 16 09:30:49.212 2023] [ 1.854500] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[Mon Oct 16 09:30:49.212 2023] [ 1.862467] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[Mon Oct 16 09:30:49.212 2023] [ 1.869802] vddpu: disabling
[Mon Oct 16 09:30:49.212 2023] [ 1.871320] cfg80211: failed to load regulatory.db
[Mon Oct 16 09:30:49.212 2023] [ 1.874144] SW4: disabling
[Mon Oct 16 09:30:49.212 2023] [ 1.881737] SWBST: disabling
[Mon Oct 16 09:30:49.212 2023] [ 1.884680] VGEN2: disabling
[Mon Oct 16 09:30:49.212 2023] [ 1.888369] ALSA device list:
[Mon Oct 16 09:30:49.212 2023] [ 1.891462] No soundcards found.
[Mon Oct 16 09:30:49.232 2023] [ 1.906248] EXT4-fs (mmcblk0p2): mounting ext3 file system using the ext4 subsystem
[Mon Oct 16 09:30:49.265 2023] [ 1.956119] EXT4-fs (mmcblk0p2): recovery complete
[Mon Oct 16 09:30:49.314 2023] [ 1.962878] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[Mon Oct 16 09:30:49.314 2023] [ 1.971284] VFS: Mounted root (ext3 filesystem) on device 179:2.
[Mon Oct 16 09:30:49.314 2023] [ 1.984545] devtmpfs: mounted
[Mon Oct 16 09:30:49.314 2023] [ 1.989562] Freeing unused kernel memory: 1024K
[Mon Oct 16 09:30:49.665 2023] [ 2.358275] systemd[1]: systemd 253.1^ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -TPM2 -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
[Mon Oct 16 09:30:49.724 2023] [ 2.390594] systemd[1]: Detected architecture arm.
[Mon Oct 16 09:30:49.724 2023]
[Mon Oct 16 09:30:49.724 2023] Welcome to NXP i.MX Release Distro 6.1-mickledore (mickledore)!
[Mon Oct 16 09:30:49.724 2023]
[Mon Oct 16 09:30:49.739 2023] [ 2.432999] systemd[1]: Hostname set to <imx6qpdlsolox>.
[Mon Oct 16 09:30:49.995 2023] [ 2.687145] systemd-sysv-generator[136]: SysV service '/etc/init.d/psplash.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[Mon Oct 16 09:30:50.068 2023] [ 2.725390] systemd-sysv-generator[136]: SysV service '/etc/init.d/reboot' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[Mon Oct 16 09:30:50.068 2023] [ 2.761878] systemd-sysv-generator[136]: SysV service '/etc/init.d/rc.local' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[Mon Oct 16 09:30:50.105 2023] [ 2.796924] systemd-sysv-generator[136]: SysV service '/etc/init.d/sshd' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[Mon Oct 16 09:30:50.229 2023] [ 2.827141] systemd-sysv-generator[136]: SysV service '/etc/init.d/umountfs' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[Mon Oct 16 09:30:50.229 2023] [ 2.856999] systemd-sysv-generator[136]: SysV service '/etc/init.d/sendsigs' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[Mon Oct 16 09:30:50.229 2023] [ 2.882139] systemd-sysv-generator[136]: SysV service '/etc/init.d/save-rtc.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[Mon Oct 16 09:30:50.234 2023] [ 2.917013] systemd-sysv-generator[136]: SysV service '/etc/init.d/halt' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[Mon Oct 16 09:30:50.314 2023] [ 2.946480] systemd-sysv-generator[136]: SysV service '/etc/init.d/single' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[Mon Oct 16 09:30:50.314 2023] [ 2.971275] systemd-sysv-generator[136]: SysV service '/etc/init.d/alignment.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[Mon Oct 16 09:30:50.329 2023] [ 3.018864] systemd-sysv-generator[136]: SysV service '/etc/init.d/umountnfs.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[Mon Oct 16 09:30:51.157 2023] [ 3.809076] systemd[1]: Queued start job for default target Graphical Interface.
[Mon Oct 16 09:30:51.157 2023] [ 3.824870] systemd[1]: Created slice Slice /system/getty.
[Mon Oct 16 09:30:51.157 2023] [ OK ] Created slice Slice /system/getty.
[Mon Oct 16 09:30:51.199 2023] [ 3.866735] systemd[1]: Created slice Slice /system/modprobe.
[Mon Oct 16 09:30:51.199 2023] [ OK ] Created slice Slice /system/modprobe.
[Mon Oct 16 09:30:51.235 2023] [ 3.902934] systemd[1]: Created slice Slice /system/serial-getty.
[Mon Oct 16 09:30:51.235 2023] [ OK ] Created slice Slice /system/serial-getty.
[Mon Oct 16 09:30:51.251 2023] [ 3.943802] systemd[1]: Created slice User and Session Slice.
[Mon Oct 16 09:30:51.274 2023] [ OK ] Created slice User and Session Slice.
[Mon Oct 16 09:30:51.288 2023] [ 3.982476] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[Mon Oct 16 09:30:51.317 2023] [ OK ] Started Dispatch Password …ts to Console Directory Watch.
[Mon Oct 16 09:30:51.352 2023] [ 4.020850] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[Mon Oct 16 09:30:51.352 2023] [ OK ] Started Forward Password R…uests to Wall Directory Watch.
[Mon Oct 16 09:30:51.367 2023] [ 4.061625] systemd[1]: Reached target Host and Network Name Lookups.
[Mon Oct 16 09:30:51.396 2023] [ OK ] Reached target Host and Network Name Lookups.
[Mon Oct 16 09:30:51.412 2023] [ 4.100921] systemd[1]: Reached target Path Units.
[Mon Oct 16 09:30:51.428 2023] [ OK ] Reached target Path Units.
[Mon Oct 16 09:30:51.462 2023] [ 4.130193] systemd[1]: Reached target Remote File Systems.
[Mon Oct 16 09:30:51.462 2023] [ OK ] Reached target Remote File Systems.
[Mon Oct 16 09:30:51.478 2023] [ 4.170993] systemd[1]: Reached target Slice Units.
[Mon Oct 16 09:30:51.499 2023] [ OK ] Reached target Slice Units.
[Mon Oct 16 09:30:51.527 2023] [ 4.200293] systemd[1]: Reached target Swaps.
[Mon Oct 16 09:30:51.527 2023] [ OK ] Reached target Swaps.
[Mon Oct 16 09:30:51.560 2023] [ 4.249555] systemd[1]: Listening on RPCbind Server Activation Socket.
[Mon Oct 16 09:30:51.582 2023] [ OK ] Listening on RPCbind Server Activation Socket.
[Mon Oct 16 09:30:51.624 2023] [ 4.291098] systemd[1]: Reached target RPC Port Mapper.
[Mon Oct 16 09:30:51.624 2023] [ OK ] Reached target RPC Port Mapper.
[Mon Oct 16 09:30:51.639 2023] [ 4.331696] systemd[1]: Listening on Syslog Socket.
[Mon Oct 16 09:30:51.660 2023] [ OK ] Listening on Syslog Socket.
[Mon Oct 16 09:30:51.707 2023] [ 4.372743] systemd[1]: Listening on initctl Compatibility Named Pipe.
[Mon Oct 16 09:30:51.707 2023] [ OK ] Listening on initctl Compatibility Named Pipe.
[Mon Oct 16 09:30:51.754 2023] [ 4.447800] systemd[1]: Journal Audit Socket was skipped because of an unmet condition check (ConditionSecurity=audit).
[Mon Oct 16 09:30:51.794 2023] [ 4.460581] systemd[1]: Listening on Journal Socket (/dev/log).
[Mon Oct 16 09:30:51.794 2023] [ OK ] Listening on Journal Socket (/dev/log).
[Mon Oct 16 09:30:51.832 2023] [ 4.503930] systemd[1]: Listening on Journal Socket.
[Mon Oct 16 09:30:51.832 2023] [ OK ] Listening on Journal Socket.
[Mon Oct 16 09:30:51.847 2023] [ 4.541849] systemd[1]: Listening on Network Service Netlink Socket.
[Mon Oct 16 09:30:51.875 2023] [ OK ] Listening on Network Service Netlink Socket.
[Mon Oct 16 09:30:51.890 2023] [ 4.584502] systemd[1]: Listening on udev Control Socket.
[Mon Oct 16 09:30:51.918 2023] [ OK ] Listening on udev Control Socket.
[Mon Oct 16 09:30:51.935 2023] [ 4.623513] systemd[1]: Listening on udev Kernel Socket.
[Mon Oct 16 09:30:51.955 2023] [ OK ] Listening on udev Kernel Socket.
[Mon Oct 16 09:30:51.971 2023] [ 4.663486] systemd[1]: Listening on User Database Manager Socket.
[Mon Oct 16 09:30:51.994 2023] [ OK ] Listening on User Database Manager Socket.
[Mon Oct 16 09:30:52.009 2023] [ 4.701334] systemd[1]: Huge Pages File System was skipped because of an unmet condition check (ConditionPathExists=/sys/kernel/mm/hugepages).
[Mon Oct 16 09:30:52.070 2023] [ 4.715153] systemd[1]: POSIX Message Queue File System was skipped because of an unmet condition check (ConditionPathExists=/proc/sys/fs/mqueue).
[Mon Oct 16 09:30:52.070 2023] [ 4.737852] systemd[1]: Mounting Kernel Debug File System...
[Mon Oct 16 09:30:52.070 2023] Mounting Kernel Debug File System...
[Mon Oct 16 09:30:52.124 2023] [ 4.770833] systemd[1]: Kernel Trace File System was skipped because of an unmet condition check (ConditionPathExists=/sys/kernel/tracing).
[Mon Oct 16 09:30:52.124 2023] [ 4.793288] systemd[1]: Mounting Temporary Directory /tmp...
[Mon Oct 16 09:30:52.124 2023] Mounting Temporary Directory /tmp...
[Mon Oct 16 09:30:52.139 2023] [ 4.833405] systemd[1]: Create List of Static Device Nodes was skipped because of an unmet condition check (ConditionFileNotEmpty=/lib/modules/4.16.0/modules.devname).
[Mon Oct 16 09:30:52.186 2023] [ 4.857853] systemd[1]: Starting Load Kernel Module configfs...
[Mon Oct 16 09:30:52.186 2023] Starting Load Kernel Module configfs...
[Mon Oct 16 09:30:52.229 2023] [ 4.902567] systemd[1]: Starting Load Kernel Module drm...
[Mon Oct 16 09:30:52.229 2023] Starting Load Kernel Module drm...
[Mon Oct 16 09:30:52.261 2023] [ 4.951970] systemd[1]: Starting Load Kernel Module fuse...
[Mon Oct 16 09:30:52.283 2023] Starting Load Kernel Module fuse...
[Mon Oct 16 09:30:52.344 2023] [ 5.017216] systemd[1]: Starting RPC Bind...
[Mon Oct 16 09:30:52.344 2023] Starting RPC Bind...
[Mon Oct 16 09:30:52.360 2023] [ 5.051182] systemd[1]: File System Check on Root Device was skipped because of an unmet condition check (ConditionPathIsReadWrite=!/).
[Mon Oct 16 09:30:52.429 2023] [ 5.066727] systemd[1]: systemd-journald.service: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[Mon Oct 16 09:30:52.429 2023] [ 5.080353] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[Mon Oct 16 09:30:52.429 2023] [ 5.097529] systemd[1]: Starting Journal Service...
[Mon Oct 16 09:30:52.429 2023] Starting Journal Service...
[Mon Oct 16 09:30:52.502 2023] [ 5.138569] systemd[1]: Load Kernel Modules was skipped because no trigger condition checks were met.
[Mon Oct 16 09:30:52.502 2023] [ 5.153665] systemd-journald[145]: Collecting audit messages is disabled.
[Mon Oct 16 09:30:52.502 2023] [ 5.155704] systemd[1]: Starting Generate network units from Kernel command line...
[Mon Oct 16 09:30:52.502 2023] Starting Generate network …ts from Kernel command line...
[Mon Oct 16 09:30:52.556 2023] [ 5.215861] systemd[1]: Starting Remount Root and Kernel File Systems...
[Mon Oct 16 09:30:52.556 2023] Starting Remount Root and Kernel File Systems...
[Mon Oct 16 09:30:52.593 2023] [ 5.266176] systemd[1]: Starting Apply Kernel Variables...
[Mon Oct 16 09:30:52.623 2023] Starting Apply Kernel Variables...
[Mon Oct 16 09:30:52.623 2023] [ 5.300934] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[Mon Oct 16 09:30:52.655 2023] [ 5.323355] systemd[1]: Starting Coldplug All udev Devices...
[Mon Oct 16 09:30:52.655 2023] Starting Coldplug All udev Devices...
[Mon Oct 16 09:30:52.693 2023] [ 5.367015] systemd[1]: Starting Setup Virtual Console...
[Mon Oct 16 09:30:52.693 2023] Starting Setup Virtual Console...
[Mon Oct 16 09:30:52.792 2023] [ 5.479118] systemd[1]: Started RPC Bind.
[Mon Oct 16 09:30:52.792 2023] [ OK ] Started RPC Bind.
[Mon Oct 16 09:30:52.849 2023] [ 5.521402] systemd[1]: Started Journal Service.
[Mon Oct 16 09:30:52.849 2023] [ OK ] Started Journal Service.
[Mon Oct 16 09:30:52.893 2023] [ OK ] Mounted Kernel Debug File System.
[Mon Oct 16 09:30:52.908 2023] [ OK ] Mounted Temporary Directory /tmp.
[Mon Oct 16 09:30:52.957 2023] [ OK ] Finished Load Kernel Module configfs.
[Mon Oct 16 09:30:53.006 2023] [ OK ] Finished Load Kernel Module drm.
[Mon Oct 16 09:30:53.062 2023] [ OK ] Finished Load Kernel Module fuse.
[Mon Oct 16 09:30:53.099 2023] [ OK ] Finished Generate network units from Kernel command line.
[Mon Oct 16 09:30:53.139 2023] [ OK ] Finished Remount Root and Kernel File Systems.
[Mon Oct 16 09:30:53.179 2023] [ OK ] Finished Apply Kernel Variables.
[Mon Oct 16 09:30:53.220 2023] [ OK ] Finished Setup Virtual Console.
[Mon Oct 16 09:30:53.251 2023] Mounting FUSE Control File System...
[Mon Oct 16 09:30:53.321 2023] Starting Flush Journal to Persistent Storage...
[Mon Oct 16 09:30:53.336 2023] Starting Create Static Device Nodes in /dev...
[Mon Oct 16 09:30:53.388 2023] [ OK ] Mounted 6.057048] systemd-journald[145]: Received client request to flush runtime journal.
[Mon Oct 16 09:30:53.388 2023] 39mFUSE Control File System.
[Mon Oct 16 09:30:53.419 2023] [ OK ] Finished Flush Journal to Persistent Storage.
[Mon Oct 16 09:30:53.475 2023] [ OK ] Finished Create Static Device Nodes in /dev.
[Mon Oct 16 09:30:53.493 2023] [ OK ] Reached target Preparation for Local File Systems.
[Mon Oct 16 09:30:53.539 2023] Mounting /var/volatile...
[Mon Oct 16 09:30:53.594 2023] Starting Rule-based Manage…for Device Events and Files...
[Mon Oct 16 09:30:53.625 2023] [ OK ] Mounted /var/volatile.
[Mon Oct 16 09:30:53.658 2023] Starting Load/Save OS Random Seed...
[Mon Oct 16 09:30:53.672 2023] [ OK ] Reached target Local File Systems.
[Mon Oct 16 09:30:53.720 2023] Starting Create Volatile Files and Directories...
[Mon Oct 16 09:30:53.801 2023] [ OK ] Finished Load/Save OS Random Seed.
[Mon Oct 16 09:30:53.828 2023] [ OK ] Started Rule-based Manager for Device Events and Files.
[Mon Oct 16 09:30:54.395 2023] [ OK ] Finished Create Volatile Files and Directories.
[Mon Oct 16 09:30:54.537 2023] [FAILED] Failed to start Network Time Synchronization.
[Mon Oct 16 09:30:54.552 2023] See 'systemctl status systemd-timesyncd.service' for details.
[Mon Oct 16 09:30:54.597 2023] [ OK ] Reached target System Time Set.
[Mon Oct 16 09:30:54.636 2023] Starting Record System Boot/Shutdown in UTMP...
[Mon Oct 16 09:30:54.731 2023] [ OK ] Finished Coldplug All udev Devices.
[Mon Oct 16 09:30:54.875 2023] Starting Start Psplash Boot Screen...
[Mon Oct 16 09:30:54.915 2023] [ OK ] Stopped Network Time Synchronization.
[Mon Oct 16 09:30:55.035 2023] [FAILED] Failed to start Network Time Synchronization.
[Mon Oct 16 09:30:55.035 2023] See 'systemctl status systemd-timesyncd.service' for details.
[Mon Oct 16 09:30:55.287 2023] [ OK ] Started Start Psplash Boot Screen.
[Mon Oct 16 09:30:55.727 2023] [ OK ] Finished Record System Boot/Shutdown in UTMP.
[Mon Oct 16 09:30:56.620 2023] [ OK ] Started Start psplash-syst…progress communication helper.
[Mon Oct 16 09:30:56.659 2023] [ OK ] Stopped Network Time Synchronization.
[Mon Oct 16 09:30:56.707 2023] [FAILED] Failed to start Network Time Synchronization.
[Mon Oct 16 09:30:56.707 2023] See 'systemctl status systemd-timesyncd.service' for details.
[Mon Oct 16 09:30:56.737 2023] [ OK ] Reached target System Initialization.
[Mon Oct 16 09:30:56.753 2023] [ OK ] Started Daily rotation of log files.
[Mon Oct 16 09:30:56.797 2023] [ OK ] Started Daily Cleanup of Temporary Directories.
[Mon Oct 16 09:30:56.828 2023] [ OK ] Reached target Timer Units.
[Mon Oct 16 09:30:56.858 2023] [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[Mon Oct 16 09:30:56.889 2023] [ OK ] Listening on D-Bus System Message Bus Socket.
[Mon Oct 16 09:30:56.904 2023] Starting sshd.socket...
[Mon Oct 16 09:30:56.935 2023] Starting Weston socket...
[Mon Oct 16 09:30:57.060 2023] Starting Console System Startup Logging...
[Mon Oct 16 09:30:57.172 2023] [ OK ] Listening on sshd.socket.
[Mon Oct 16 09:30:57.198 2023] [ OK ] Listening on Weston socket.
[Mon Oct 16 09:30:57.212 2023] [ OK ] Reached target Socket Units.
[Mon Oct 16 09:30:57.229 2023] [ OK ] Reached target Basic System.
[Mon Oct 16 09:30:57.307 2023] [ OK ] Started Job spooling tools.
[Mon Oct 16 09:30:57.346 2023] [ OK ] Started Periodic Command Scheduler.
[Mon Oct 16 09:30:57.395 2023] Starting D-Bus System Message Bus...
[Mon Oct 16 09:30:57.426 2023] [ OK ] Started Linux Firmware Loader Daemon.
[Mon Oct 16 09:30:57.517 2023] [ OK ] Started Configuration for i.MX GPU (Former rc_gpu.S).
[Mon Oct 16 09:30:57.580 2023] Starting IPv6 Packet Filtering Framework...
[Mon Oct 16 09:30:57.639 2023] Starting IPv4 Packet Filtering Framework...
[Mon Oct 16 09:30:57.687 2023] Starting Telephony service...
[Mon Oct 16 09:30:57.736 2023] [ OK ] Started Updates psplash to basic.
[Mon Oct 16 09:30:57.827 2023] Starting LSB: Run /etc/rc.local if it exist...
[Mon Oct 16 09:30:57.901 2023] [ OK ] Started System Logging Service.
[Mon Oct 16 09:30:57.964 2023] [FAILED] Failed to start User Login Management.
[Mon Oct 16 09:30:57.995 2023] See 'systemctl status systemd-logind.service' for details.
[Mon Oct 16 09:30:58.011 2023] [ OK ] Stopped Network Time Synchronization.
[Mon Oct 16 09:30:58.063 2023] syslogd[460]: Error opening log file: /var/log/auth.log: No such file or directory
[Mon Oct 16 09:30:58.063 2023] syslogd[460]: Error opening log file: /var/log/syslog: No such file or directory
[Mon Oct 16 09:30:58.079 2023] syslogd[460]: Error opening log file: /var/log/kern.log: No such file or directory
[Mon Oct 16 09:30:58.133 2023] syslogd[460]: Error opening log file: /var/log/mail.log: No such file or directory
[Mon Oct 16 09:30:58.133 2023] [FAILED] Failed to start Network Time Synchronization.
[Mon Oct 16 09:30:58.147 2023] See 'systemctl status systemd-timesyncd.service' for details.
[Mon Oct 16 09:30:58.170 2023] syslogd[460]: Error opening log file: /var/log/mail.err: No such file or directory
[Mon Oct 16 09:30:58.206 2023] syslogd[460]: Error opening log file: /var/log/messages: No such file or directory
[Mon Oct 16 09:30:58.222 2023] [ OK ] Started TEE Supplicant.
[Mon Oct 16 09:30:58.254 2023] Starting OpenSSH Key Generation...
[Mon Oct 16 09:30:58.397 2023] [ OK ] Started D-Bus System Message Bus.
[Mon Oct 16 09:30:58.610 2023] [FAILED] Failed to start Console System Startup Logging.
[Mon Oct 16 09:30:58.626 2023] See 'systemctl status console-kit-log-system-start.service' for details.
[Mon Oct 16 09:30:58.679 2023] [ OK ] Finished IPv6 Packet Filtering Framework.
[Mon Oct 16 09:30:58.700 2023] [ OK ] Finished IPv4 Packet Filtering Framework.
[Mon Oct 16 09:30:58.769 2023] [ OK ] Started LSB: Run /etc/rc.local if it exist.
[Mon Oct 16 09:30:58.936 2023] [ OK ] Reached target Preparation for Network.
[Mon Oct 16 09:30:58.967 2023] Starting Connection service...
[Mon Oct 16 09:30:59.008 2023] [ OK ] Stopped User Login Management.
[Mon Oct 16 09:30:59.022 2023] Starting Load Kernel Module drm...
[Mon Oct 16 09:30:59.134 2023] Starting Network Configuration...
[Mon Oct 16 09:30:59.165 2023] [ OK ] Stopped Network Time Synchronization.
[Mon Oct 16 09:30:59.251 2023] [FAILED] Failed to start Network Time Synchronization.
[Mon Oct 16 09:30:59.297 2023] See 'systemctl status systemd-timesyncd.service' for details.
[Mon Oct 16 09:30:59.328 2023] [ OK ] Finished Load Kernel Module drm.
[Mon Oct 16 09:30:59.566 2023] [ OK ] Finished OpenSSH Key Generation.
[Mon Oct 16 09:30:59.614 2023] [ OK ] Started Telephony service.
[Mon Oct 16 09:30:59.958 2023] [ OK ] Created slice Slice /system/systemd-fsck.
[Mon Oct 16 09:31:00.034 2023] Starting File System Check on /dev/mmcblk0p1...
[Mon Oct 16 09:31:00.066 2023] [FAILED] Failed to start User Login Management.
[Mon Oct 16 09:31:00.098 2023] See 'systemctl status systemd-logind.service' for details.
[Mon Oct 16 09:31:00.128 2023] [ OK ] Stopped Network Time Synchronization.
[Mon Oct 16 09:31:00.158 2023] [FAILED] Failed to start Network Time Synchronization.
[Mon Oct 16 09:31:00.186 2023] See 'systemctl status systemd-timesyncd.service' for details.
[Mon Oct 16 09:31:00.265 2023] [ OK ] Listening on Load/Save RF …itch Status /dev/rfkill Watch.
[Mon Oct 16 09:31:00.265 2023] [ OK ] Stopped User Login Management.
[Mon Oct 16 09:31:00.265 2023] Starting Load Kernel Module drm...
[Mon Oct 16 09:31:00.328 2023] [ OK ] Finished Load Kernel Module drm.
[Mon Oct 16 09:31:00.376 2023] [FAILED] Failed to start User Login Management.
[Mon Oct 16 09:31:00.412 2023] See 'systemctl status systemd-logind.service' for details.
[Mon Oct 16 09:31:00.450 2023] [ OK ] Finished File System Check on /dev/mmcblk0p1.
[Mon Oct 16 09:31:00.491 2023] [ OK ] Started Connection service.
[Mon Oct 16 09:31:00.521 2023] Mounting /run/media/mmcblk0p1...
[Mon Oct 16 09:31:00.569 2023] Starting Avahi mDNS/DNS-SD Stack...
[Mon Oct 16 09:31:00.618 2023] [ OK ] Stopped User Login Management.
[Mon Oct 16 09:31:00.650 2023] Starting Load Kernel Module drm...
[Mon Oct 16 09:31:00.681 2023] [ OK ] Started Network Configuration.
[Mon Oct 16 09:31:00.736 2023] [ OK ] Mounted /run/media/mmcblk0p1.
[Mon Oct 16 09:31:00.778 2023] [ OK ] Finished Load Kernel Module drm.
[Mon Oct 16 09:31:00.852 2023] [ OK ] Started Avahi mDNS/DNS-SD Stack.
[Mon Oct 16 09:31:00.909 2023] [FAILED] Failed to start Hostname Service.
[Mon Oct 16 09:31:00.947 2023] See 'systemctl status systemd-hostnamed.service' for details.
[Mon Oct 16 09:31:00.979 2023] [FAILED] Failed to start User Login Management.
[Mon Oct 16 09:31:01.016 2023] See 'systemctl status systemd-logind.service' for details.
[Mon Oct 16 09:31:01.064 2023] Starting WPA supplicant...
[Mon Oct 16 09:31:01.096 2023] [ OK ] Stopped User Login Management.
[Mon Oct 16 09:31:01.161 2023] Starting Load Kernel Module drm...
[Mon Oct 16 09:31:01.217 2023] [ OK ] Finished Load Kernel Module drm.
[Mon Oct 16 09:31:01.217 2023] [ OK ] Started WPA supplicant.
[Mon Oct 16 09:31:01.233 2023] [ OK ] Reached target Network.
[Mon Oct 16 09:31:01.305 2023] [ OK ] Started NFS status monitor for NFSv2/3 locking..
[Mon Oct 16 09:31:01.336 2023] Starting Network Time Service...
[Mon Oct 16 09:31:01.389 2023] [ OK ] Started Update psplash to network.
[Mon Oct 16 09:31:01.404 2023] Starting Terminate Psplash Boot Screen...
[Mon Oct 16 09:31:01.458 2023] Starting /etc/rc.local Compatibility...
[Mon Oct 16 09:31:01.514 2023] [FAILED] Failed to start User Login Management.
[Mon Oct 16 09:31:01.546 2023] See 'systemctl status systemd-logind.service' for details.
[Mon Oct 16 09:31:01.594 2023] Starting Permit User Sessions...
[Mon Oct 16 09:31:01.642 2023] [ OK ] Started Network Time Service.
[Mon Oct 16 09:31:01.706 2023] [FAILED] Failed to start Terminate Psplash Boot Screen.
[Mon Oct 16 09:31:01.737 2023] See 'systemctl status psplash-quit.service' for details.
[Mon Oct 16 09:31:01.797 2023] [ OK ] Started /etc/rc.local Compatibility.
[Mon Oct 16 09:31:01.812 2023] [ OK ] Finished Permit User Sessions.
[Mon Oct 16 09:31:01.878 2023] [ OK ] Started Getty on tty1.
[Mon Oct 16 09:31:01.949 2023] [ OK ] Started Serial Getty on ttymxc0.
[Mon Oct 16 09:31:01.979 2023] [ OK ] Reached target Login Prompts.
[Mon Oct 16 09:31:02.018 2023] [ OK ] Stopped User Login Management.
[Mon Oct 16 09:31:02.066 2023] Starting Load Kernel Module drm...
[Mon Oct 16 09:31:02.099 2023] Starting Weston, a Wayland…ositor, as a system service...
[Mon Oct 16 09:31:02.169 2023] [ OK ] Finished Load Kernel Module drm.
[Mon Oct 16 09:31:02.169 2023] [FAILED] Failed to start User Login Management.
[Mon Oct 16 09:31:02.185 2023] See 'systemctl status systemd-logind.service' for details.
[Mon Oct 16 09:31:02.229 2023] [ OK ] Reached target Multi-User System.
[Mon Oct 16 09:31:02.261 2023] Starting User Database Manager...
[Mon Oct 16 09:31:02.972 2023] [ OK ] Started User Database Manager.
[Mon Oct 16 09:31:03.171 2023] [FAILED] Failed to start Weston, a …mpositor, as a system service.
[Mon Oct 16 09:31:03.187 2023] See 'systemctl status weston.service' for details.
[Mon Oct 16 09:31:03.251 2023] [ OK ] Reached target Graphical Interface.
[Mon Oct 16 09:31:03.295 2023] Starting Record Runlevel Change in UTMP...
[Mon Oct 16 09:31:03.343 2023] [ OK ] Finished Record Runlevel Change in UTMP.
[Mon Oct 16 09:31:04.444 2023]
[Mon Oct 16 09:31:04.444 2023] NXP i.MX Release Distro 6.1-mickledore imx6qpdlsolox ttymxc0
[Mon Oct 16 09:31:04.444 2023]
[Mon Oct 16 09:31:04.444 2023] imx6qpdlsolox login: root
[Mon Oct 16 09:31:06.860 2023] root@imx6qpdlsolox:~#
[Mon Oct 16 09:31:06.987 2023] root@imx6qpdlsolox:~#

 

===============================================================================

2. over 4.17 version, rootfs mounting fail and the board is stopped. I also tried at 4.19& 5.15 & 6.1 version. it has the same result.

[Mon Oct 16 09:45:17.769 2023] U-Boot 2023.07-00800-g247aa5a191-dirty (Oct 13 2023 - 11:49:24 +0900)
[Mon Oct 16 09:45:17.769 2023]
[Mon Oct 16 09:45:17.769 2023] CPU: Freescale i.MX6DP rev1.1 996 MHz (running at 792 MHz)
[Mon Oct 16 09:45:17.769 2023] CPU: Automotive temperature grade (-40C to 125C) at 36C
[Mon Oct 16 09:45:17.769 2023] Reset cause: POR
[Mon Oct 16 09:45:17.769 2023] Model: Freescale i.MX6 DualPlus Board
[Mon Oct 16 09:45:17.769 2023] Board: MX6Q-Sabreauto rev@
[Mon Oct 16 09:45:17.769 2023] DRAM: 1 GiB
[Mon Oct 16 09:45:17.816 2023] SETUP SPI...
[Mon Oct 16 09:45:18.846 2023] Core: 65 devices, 15 uclasses, devicetree: separate
[Mon Oct 16 09:45:18.846 2023] PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x21
[Mon Oct 16 09:45:18.846 2023] Flash: ## Unknown flash on Bank 1 - Size = 0x00000000 = 0 MB
[Mon Oct 16 09:45:18.846 2023] 0 Bytes
[Mon Oct 16 09:45:18.846 2023] NAND: 1024 MiB
[Mon Oct 16 09:45:18.861 2023] MMC:eMMC board_emmc_init...
[Mon Oct 16 09:45:18.882 2023] cfg->b_max:65535 cfg->f_min:400000 cfg->f_max:52000000
[Mon Oct 16 09:45:18.882 2023] FSL_SDHC: 0
[Mon Oct 16 09:45:18.882 2023] Loading Environment from MMC... at the mmc_startup
[Mon Oct 16 09:45:19.025 2023] *** Warning - bad CRC, using default environment
[Mon Oct 16 09:45:19.025 2023]
[Mon Oct 16 09:45:19.025 2023] Loading Environment from nowhere... OK
[Mon Oct 16 09:45:19.025 2023] In: serial@02020000
[Mon Oct 16 09:45:19.025 2023] Out: serial@02020000
[Mon Oct 16 09:45:19.025 2023] Err: serial@02020000
[Mon Oct 16 09:45:19.137 2023] SEC0: RNG instantiated
[Mon Oct 16 09:45:19.270 2023] switch to partitions #0, OK
[Mon Oct 16 09:45:19.270 2023] mmc0(part 0) is current device
[Mon Oct 16 09:45:19.270 2023] Net: eth0: ethernet@2188000 [PRIME]
[Mon Oct 16 09:45:19.378 2023] Hit any key to stop autoboot: 1 0
[Mon Oct 16 09:45:19.378 2023] STU iMX6 # setenv console "ttymxc0,115200"
[Mon Oct 16 09:45:23.410 2023] STU iMX6 # setenv bootargs "console=${console} root=/dev/mmcblk0p2 rootwait rw"
[Mon Oct 16 09:45:29.458 2023] STU iMX6 # setenv bootcmd "run bootargs; bootz ${loadaddr} - ${fdt_addr}"
[Mon Oct 16 09:45:33.463 2023] STU iMX6 # run bootcmd
[Mon Oct 16 09:45:37.204 2023] Unknown command 'rootwait' - try 'help'
[Mon Oct 16 09:45:37.204 2023] Kernel image @ 0x12000000 [ 0x000000 - 0x71fb40 ]
[Mon Oct 16 09:45:37.204 2023] ## Flattened Device Tree blob at 18000000
[Mon Oct 16 09:45:37.204 2023] Booting using the fdt blob at 0x18000000
[Mon Oct 16 09:45:37.204 2023] Working FDT set to 18000000
[Mon Oct 16 09:45:37.204 2023] Using Device Tree in place at 18000000, end 1800a6a7
[Mon Oct 16 09:45:37.204 2023] Working FDT set to 18000000
[Mon Oct 16 09:45:37.204 2023]
[Mon Oct 16 09:45:37.204 2023] Starting kernel ...
[Mon Oct 16 09:45:37.204 2023]
[Mon Oct 16 09:45:38.325 2023] [ 0.000000] Booting Linux on physical CPU 0x0
[Mon Oct 16 09:45:38.325 2023] [ 0.000000] Linux version 4.17.0-rc1 (aryz@csintech-linux) (gcc version 11.3.0 (GCC)) #1 SMP Mon Oct 16 09:35:21 KST 2023
[Mon Oct 16 09:45:38.325 2023] [ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d
[Mon Oct 16 09:45:38.325 2023] [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[Mon Oct 16 09:45:38.325 2023] [ 0.000000] OF: fdt: Machine model: Freescale i.MX6 DualPlus Board
[Mon Oct 16 09:45:38.325 2023] [ 0.000000] Memory policy: Data cache writealloc
[Mon Oct 16 09:45:38.325 2023] [ 0.000000] Reserved memory: created CMA memory pool at 0x3c000000, size 320 MiB
[Mon Oct 16 09:45:38.325 2023] [ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[Mon Oct 16 09:45:38.325 2023] [ 0.000000] random: get_random_bytes called from start_kernel+0x8c/0x418 with crng_init=0
[Mon Oct 16 09:45:38.325 2023] [ 0.000000] percpu: Embedded 16 pages/cpu @(ptrval) s36392 r8192 d20952 u65536
[Mon Oct 16 09:45:38.325 2023] [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 260608
[Mon Oct 16 09:45:38.325 2023] [ 0.000000] Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait rw
[Mon Oct 16 09:45:38.325 2023] [ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[Mon Oct 16 09:45:38.341 2023] [ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[Mon Oct 16 09:45:38.341 2023] [ 0.000000] Memory: 688156K/1048576K available (10240K kernel code, 498K rwdata, 3156K rodata, 1024K init, 7638K bss, 32740K reserved, 327680K cma-reserved, 0K highmem)
[Mon Oct 16 09:45:38.341 2023] [ 0.000000] Virtual kernel memory layout:
[Mon Oct 16 09:45:38.341 2023] [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[Mon Oct 16 09:45:38.341 2023] [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[Mon Oct 16 09:45:38.341 2023] [ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[Mon Oct 16 09:45:38.341 2023] [ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[Mon Oct 16 09:45:38.341 2023] [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[Mon Oct 16 09:45:38.341 2023] [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[Mon Oct 16 09:45:38.341 2023] [ 0.000000] .text : 0x(ptrval) - 0x(ptrval) (11232 kB)
[Mon Oct 16 09:45:38.341 2023] [ 0.000000] .init : 0x(ptrval) - 0x(ptrval) (1024 kB)
[Mon Oct 16 09:45:38.341 2023] [ 0.000000] .data : 0x(ptrval) - 0x(ptrval) ( 499 kB)
[Mon Oct 16 09:45:38.341 2023] [ 0.000000] .bss : 0x(ptrval) - 0x(ptrval) (7639 kB)
[Mon Oct 16 09:45:38.358 2023] [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[Mon Oct 16 09:45:38.358 2023] [ 0.000000] Running RCU self tests
[Mon Oct 16 09:45:38.358 2023] [ 0.000000] Hierarchical RCU implementation.
[Mon Oct 16 09:45:38.358 2023] [ 0.000000] RCU event tracing is enabled.
[Mon Oct 16 09:45:38.358 2023] [ 0.000000] RCU lockdep checking is enabled.
[Mon Oct 16 09:45:38.358 2023] [ 0.000000] RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
[Mon Oct 16 09:45:38.358 2023] [ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[Mon Oct 16 09:45:38.358 2023] [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[Mon Oct 16 09:45:38.358 2023] [ 0.000000] L2C-310 erratum 769419 enabled
[Mon Oct 16 09:45:38.358 2023] [ 0.000000] L2C-310 enabling early BRESP for Cortex-A9
[Mon Oct 16 09:45:38.358 2023] [ 0.000000] L2C-310 full line of zeros enabled for Cortex-A9
[Mon Oct 16 09:45:38.358 2023] [ 0.000000] L2C-310 ID prefetch enabled, offset 16 lines
[Mon Oct 16 09:45:38.358 2023] [ 0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled
[Mon Oct 16 09:45:38.358 2023] [ 0.000000] L2C-310 cache controller enabled, 16 ways, 1024 kB
[Mon Oct 16 09:45:38.358 2023] [ 0.000000] L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76470001
[Mon Oct 16 09:45:38.358 2023] [ 0.000000] Switching to timer-based delay loop, resolution 15ns
[Mon Oct 16 09:45:38.358 2023] [ 0.000008] sched_clock: 32 bits at 66MHz, resolution 15ns, wraps every 32537631224ns
[Mon Oct 16 09:45:38.367 2023] [ 0.000034] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 28958491609 ns
[Mon Oct 16 09:45:38.367 2023] [ 0.001076] Console: colour dummy device 80x30
[Mon Oct 16 09:45:38.367 2023] [ 0.001105] Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar
[Mon Oct 16 09:45:38.367 2023] [ 0.001122] ... MAX_LOCKDEP_SUBCLASSES: 8
[Mon Oct 16 09:45:38.367 2023] [ 0.001138] ... MAX_LOCK_DEPTH: 48
[Mon Oct 16 09:45:38.367 2023] [ 0.001154] ... MAX_LOCKDEP_KEYS: 8191
[Mon Oct 16 09:45:38.367 2023] [ 0.001170] ... CLASSHASH_SIZE: 4096
[Mon Oct 16 09:45:38.367 2023] [ 0.001185] ... MAX_LOCKDEP_ENTRIES: 32768
[Mon Oct 16 09:45:38.367 2023] [ 0.001201] ... MAX_LOCKDEP_CHAINS: 65536
[Mon Oct 16 09:45:38.367 2023] [ 0.001216] ... CHAINHASH_SIZE: 32768
[Mon Oct 16 09:45:38.367 2023] [ 0.001231] memory used by lock dependency info: 4655 kB
[Mon Oct 16 09:45:38.367 2023] [ 0.001247] per task-struct memory footprint: 1536 bytes
[Mon Oct 16 09:45:38.367 2023] [ 0.001295] Calibrating delay loop (skipped), value calculated using timer frequency.. 132.00 BogoMIPS (lpj=660000)
[Mon Oct 16 09:45:38.367 2023] [ 0.001327] pid_max: default: 32768 minimum: 301
[Mon Oct 16 09:45:38.670 2023] [ 0.001631] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[Mon Oct 16 09:45:38.670 2023] [ 0.001666] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[Mon Oct 16 09:45:38.670 2023] [ 0.003239] CPU: Testing write buffer coherency: ok
[Mon Oct 16 09:45:38.670 2023] [ 0.004013] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[Mon Oct 16 09:45:38.670 2023] [ 0.005399] Setting up static identity map for 0x10100000 - 0x10100078
[Mon Oct 16 09:45:38.670 2023] [ 0.005789] Hierarchical SRCU implementation.
[Mon Oct 16 09:45:38.670 2023] [ 0.007249] smp: Bringing up secondary CPUs ...
[Mon Oct 16 09:45:38.670 2023] [ 0.008962] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[Mon Oct 16 09:45:38.670 2023] [ 0.009513] smp: Brought up 1 node, 2 CPUs
[Mon Oct 16 09:45:38.670 2023] [ 0.009546] SMP: Total of 2 processors activated (264.00 BogoMIPS).
[Mon Oct 16 09:45:38.670 2023] [ 0.009564] CPU: All CPU(s) started in SVC mode.
[Mon Oct 16 09:45:38.670 2023] [ 0.011624] devtmpfs: initialized
[Mon Oct 16 09:45:38.670 2023] [ 0.043521] Built 1 zonelists, mobility grouping on. Total pages: 253959
[Mon Oct 16 09:45:38.670 2023] [ 0.043883] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[Mon Oct 16 09:45:38.670 2023] [ 0.045774] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[Mon Oct 16 09:45:38.684 2023] [ 0.045818] futex hash table entries: 512 (order: 3, 32768 bytes)
[Mon Oct 16 09:45:38.684 2023] [ 0.046299] pinctrl core: initialized pinctrl subsystem
[Mon Oct 16 09:45:38.684 2023] [ 0.049474] NET: Registered protocol family 16
[Mon Oct 16 09:45:38.684 2023] [ 0.064136] DMA: preallocated 256 KiB pool for atomic coherent allocations
[Mon Oct 16 09:45:38.684 2023] [ 0.066786] cpuidle: using governor menu
[Mon Oct 16 09:45:38.684 2023] [ 0.066954] CPU identified as i.MX6Q, silicon rev 2.1
[Mon Oct 16 09:45:38.684 2023] [ 0.077975] vdd1p1: supplied by regulator-dummy
[Mon Oct 16 09:45:38.684 2023] [ 0.079269] vdd3p0: supplied by regulator-dummy
[Mon Oct 16 09:45:38.684 2023] [ 0.080400] vdd2p5: supplied by regulator-dummy
[Mon Oct 16 09:45:38.684 2023] [ 0.081531] vddarm: supplied by regulator-dummy
[Mon Oct 16 09:45:38.684 2023] [ 0.082691] vddpu: supplied by regulator-dummy
[Mon Oct 16 09:45:38.684 2023] [ 0.090701] vddsoc: supplied by regulator-dummy
[Mon Oct 16 09:45:38.684 2023] [ 0.103432] No ATAGs?
[Mon Oct 16 09:45:38.684 2023] [ 0.103673] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[Mon Oct 16 09:45:38.684 2023] [ 0.103742] hw-breakpoint: maximum watchpoint size is 4 bytes.
[Mon Oct 16 09:45:38.684 2023] [ 0.105984] imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[Mon Oct 16 09:45:38.684 2023] [ 0.157574] mxs-dma 110000.dma-apbh: initialized
[Mon Oct 16 09:45:38.699 2023] [ 0.160484] vgaarb: loaded
[Mon Oct 16 09:45:38.699 2023] [ 0.161368] SCSI subsystem initialized
[Mon Oct 16 09:45:38.699 2023] [ 0.162413] usbcore: registered new interface driver usbfs
[Mon Oct 16 09:45:38.699 2023] [ 0.162575] usbcore: registered new interface driver hub
[Mon Oct 16 09:45:38.699 2023] [ 0.162766] usbcore: registered new device driver usb
[Mon Oct 16 09:45:38.699 2023] [ 0.165530] i2c i2c-0: IMX I2C adapter registered
[Mon Oct 16 09:45:38.699 2023] [ 0.165571] i2c i2c-0: can't use DMA, using PIO instead.
[Mon Oct 16 09:45:38.699 2023] [ 0.166925] i2c i2c-1: IMX I2C adapter registered
[Mon Oct 16 09:45:38.699 2023] [ 0.166962] i2c i2c-1: can't use DMA, using PIO instead.
[Mon Oct 16 09:45:38.699 2023] [ 0.168231] i2c i2c-2: IMX I2C adapter registered
[Mon Oct 16 09:45:38.699 2023] [ 0.168268] i2c i2c-2: can't use DMA, using PIO instead.
[Mon Oct 16 09:45:38.699 2023] [ 0.168477] media: Linux media interface: v0.10
[Mon Oct 16 09:45:38.699 2023] [ 0.168581] Linux video capture interface: v2.00
[Mon Oct 16 09:45:38.699 2023] [ 0.168926] pps_core: LinuxPPS API ver. 1 registered
[Mon Oct 16 09:45:38.699 2023] [ 0.168947] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[Mon Oct 16 09:45:38.699 2023] [ 0.168998] PTP clock support registered
[Mon Oct 16 09:45:38.699 2023] [ 0.169815] Advanced Linux Sound Architecture Driver Initialized.
[Mon Oct 16 09:45:38.699 2023] [ 0.171651] Bluetooth: Core ver 2.22
[Mon Oct 16 09:45:38.708 2023] [ 0.171799] NET: Registered protocol family 31
[Mon Oct 16 09:45:38.708 2023] [ 0.171819] Bluetooth: HCI device and connection manager initialized
[Mon Oct 16 09:45:38.708 2023] [ 0.171894] Bluetooth: HCI socket layer initialized
[Mon Oct 16 09:45:38.708 2023] [ 0.171927] Bluetooth: L2CAP socket layer initialized
[Mon Oct 16 09:45:38.708 2023] [ 0.172081] Bluetooth: SCO socket layer initialized
[Mon Oct 16 09:45:38.708 2023] [ 0.173394] clocksource: Switched to clocksource mxc_timer1
[Mon Oct 16 09:45:38.708 2023] [ 0.173946] VFS: Disk quotas dquot_6.6.0
[Mon Oct 16 09:45:38.708 2023] [ 0.174094] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[Mon Oct 16 09:45:38.708 2023] [ 0.198087] NET: Registered protocol family 2
[Mon Oct 16 09:45:38.708 2023] [ 0.199644] tcp_listen_portaddr_hash hash table entries: 512 (order: 2, 20480 bytes)
[Mon Oct 16 09:45:38.708 2023] [ 0.199857] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[Mon Oct 16 09:45:38.708 2023] [ 0.200005] TCP bind hash table entries: 8192 (order: 6, 294912 bytes)
[Mon Oct 16 09:45:38.708 2023] [ 0.202651] TCP: Hash tables configured (established 8192 bind 8192)
[Mon Oct 16 09:45:38.708 2023] [ 0.203110] UDP hash table entries: 512 (order: 3, 40960 bytes)
[Mon Oct 16 09:45:38.854 2023] [ 0.203626] UDP-Lite hash table entries: 512 (order: 3, 40960 bytes)
[Mon Oct 16 09:45:38.854 2023] [ 0.204329] NET: Registered protocol family 1
[Mon Oct 16 09:45:38.854 2023] [ 0.205796] RPC: Registered named UNIX socket transport module.
[Mon Oct 16 09:45:38.854 2023] [ 0.205842] RPC: Registered udp transport module.
[Mon Oct 16 09:45:38.854 2023] [ 0.205862] RPC: Registered tcp transport module.
[Mon Oct 16 09:45:38.854 2023] [ 0.205882] RPC: Registered tcp NFSv4.1 backchannel transport module.
[Mon Oct 16 09:45:38.854 2023] [ 0.208252] hw perfevents: no interrupt-affinity property for /soc/pmu, guessing.
[Mon Oct 16 09:45:38.854 2023] [ 0.208726] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
[Mon Oct 16 09:45:38.854 2023] [ 0.212008] Initialise system trusted keyrings
[Mon Oct 16 09:45:38.854 2023] [ 0.212556] workingset: timestamp_bits=30 max_order=18 bucket_order=0
[Mon Oct 16 09:45:38.854 2023] [ 0.227182] NFS: Registering the id_resolver key type
[Mon Oct 16 09:45:38.854 2023] [ 0.227295] Key type id_resolver registered
[Mon Oct 16 09:45:38.854 2023] [ 0.227342] Key type id_legacy registered
[Mon Oct 16 09:45:38.854 2023] [ 0.227470] jffs2: version 2.2. (NAND) ⓒ 2001-2006 Red Hat, Inc.
[Mon Oct 16 09:45:38.854 2023] [ 0.228752] fuse init (API version 7.26)
[Mon Oct 16 09:45:38.854 2023] [ 0.230213] random: fast init done
[Mon Oct 16 09:45:38.854 2023] [ 0.238812] Key type asymmetric registered
[Mon Oct 16 09:45:38.869 2023] [ 0.238917] Asymmetric key parser 'x509' registered
[Mon Oct 16 09:45:38.869 2023] [ 0.239096] bounce: pool size: 64 pages
[Mon Oct 16 09:45:38.869 2023] [ 0.239187] io scheduler noop registered
[Mon Oct 16 09:45:38.869 2023] [ 0.239208] io scheduler deadline registered
[Mon Oct 16 09:45:38.869 2023] [ 0.239294] io scheduler cfq registered (default)
[Mon Oct 16 09:45:38.869 2023] [ 0.239318] io scheduler mq-deadline registered
[Mon Oct 16 09:45:38.869 2023] [ 0.239337] io scheduler kyber registered
[Mon Oct 16 09:45:38.869 2023] [ 0.245443] imx-sdma 20ec000.sdma: Direct firmware load for imx/sdma/sdma-imx6q.bin failed with error -2
[Mon Oct 16 09:45:38.869 2023] [ 0.245560] imx-sdma 20ec000.sdma: external firmware not found, using ROM firmware
[Mon Oct 16 09:45:38.869 2023] [ 0.251850] imx-gpc 20dc000.gpc: more than 6 clocks
[Mon Oct 16 09:45:38.869 2023] [ 0.252571] imx-gpc: probe of 20dc000.gpc failed with error -22
[Mon Oct 16 09:45:38.869 2023] [ 0.255718] pfuze100-regulator 0-0008: Full layer: 2, Metal layer: 1
[Mon Oct 16 09:45:38.869 2023] [ 0.256563] pfuze100-regulator 0-0008: FAB: 0, FIN: 0
[Mon Oct 16 09:45:38.869 2023] [ 0.256587] pfuze100-regulator 0-0008: pfuze100 found.
[Mon Oct 16 09:45:38.869 2023] [ 0.280685] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 22, base_baud = 5000000) is a IMX
[Mon Oct 16 09:45:38.869 2023] [ 1.149947] console [ttymxc0] enabled
[Mon Oct 16 09:45:38.878 2023] [ 1.182844] brd: module loaded
[Mon Oct 16 09:45:38.894 2023] [ 1.210385] loop: module loaded
[Mon Oct 16 09:45:38.918 2023] [ 1.215960] at24 0-0050: 131072 byte 24c1024 EEPROM, writable, 1 bytes/write
[Mon Oct 16 09:45:39.008 2023] [ 1.238406] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xd3
[Mon Oct 16 09:45:39.008 2023] [ 1.244833] nand: Micron MT29F8G08ABACAWP
[Mon Oct 16 09:45:39.008 2023] [ 1.248866] nand: 1024 MiB, SLC, erase size: 256 KiB, page size: 4096, OOB size: 224
[Mon Oct 16 09:45:39.008 2023] [ 1.258446] Bad block table found at page 262080, version 0x01
[Mon Oct 16 09:45:39.008 2023] [ 1.264804] Bad block table found at page 262016, version 0x01
[Mon Oct 16 09:45:39.008 2023] [ 1.274534] gpmi-nand 112000.gpmi-nand: driver registered.
[Mon Oct 16 09:45:39.008 2023] [ 1.284024] spi_imx 2008000.spi: probed
[Mon Oct 16 09:45:39.008 2023] [ 1.289180] libphy: Fixed MDIO Bus: probed
[Mon Oct 16 09:45:39.008 2023] [ 1.294440] CAN device driver interface
[Mon Oct 16 09:45:39.008 2023] [ 1.302078] fec 2188000.ethernet: 2188000.ethernet supply phy not found, using dummy regulator
[Mon Oct 16 09:45:39.119 2023] [ 1.424744] pps pps0: new PPS source ptp0
[Mon Oct 16 09:45:39.231 2023] [ 1.455095] libphy: fec_enet_mii_bus: probed
[Mon Oct 16 09:45:39.231 2023] [ 1.460702] fec 2188000.ethernet eth0: registered PHC device 0
[Mon Oct 16 09:45:39.231 2023] [ 1.467834] usbcore: registered new interface driver asix
[Mon Oct 16 09:45:39.231 2023] [ 1.473414] usbcore: registered new interface driver ax88179_178a
[Mon Oct 16 09:45:39.231 2023] [ 1.479614] usbcore: registered new interface driver cdc_ether
[Mon Oct 16 09:45:39.231 2023] [ 1.486351] usbcore: registered new interface driver net1080
[Mon Oct 16 09:45:39.231 2023] [ 1.492130] usbcore: registered new interface driver cdc_subset
[Mon Oct 16 09:45:39.231 2023] [ 1.498216] usbcore: registered new interface driver zaurus
[Mon Oct 16 09:45:39.231 2023] [ 1.504022] usbcore: registered new interface driver cdc_ncm
[Mon Oct 16 09:45:39.231 2023] [ 1.509704] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[Mon Oct 16 09:45:39.231 2023] [ 1.516295] ehci-pci: EHCI PCI platform driver
[Mon Oct 16 09:45:39.231 2023] [ 1.520847] ehci-mxc: Freescale On-Chip EHCI Host driver
[Mon Oct 16 09:45:39.231 2023] [ 1.526786] usbcore: registered new interface driver usb-storage
[Mon Oct 16 09:45:39.231 2023] [ 1.544159] rtc-ds1307 2-0068: registered as rtc0
[Mon Oct 16 09:45:39.293 2023] [ 1.550443] i2c /dev entries driver
[Mon Oct 16 09:45:39.293 2023] [ 1.559482] imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
[Mon Oct 16 09:45:39.293 2023] [ 1.565973] Bluetooth: HCI UART driver ver 2.3
[Mon Oct 16 09:45:39.293 2023] [ 1.570448] Bluetooth: HCI UART protocol H4 registered
[Mon Oct 16 09:45:39.293 2023] [ 1.576050] Bluetooth: HCI UART protocol LL registered
[Mon Oct 16 09:45:39.293 2023] [ 1.582176] sdhci: Secure Digital Host Controller Interface driver
[Mon Oct 16 09:45:39.293 2023] [ 1.588430] sdhci: Copyright(c) Pierre Ossman
[Mon Oct 16 09:45:39.293 2023] [ 1.592808] sdhci-pltfm: SDHCI platform and OF driver helper
[Mon Oct 16 09:45:39.354 2023] [ 1.634785] mmc0: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
[Mon Oct 16 09:45:39.354 2023] [ 1.646612] caam 2100000.crypto: device ID = 0x0a16010000000000 (Era -524)
[Mon Oct 16 09:45:39.354 2023] [ 1.653570] caam 2100000.crypto: job rings = 2, qi = 0, dpaa2 = no
[Mon Oct 16 09:45:39.530 2023] [ 1.673579] caam algorithms registered in /proc/crypto
[Mon Oct 16 09:45:39.530 2023] [ 1.683851] caam_jr 2101000.jr: registering rng-caam
[Mon Oct 16 09:45:39.530 2023] [ 1.689913] usbcore: registered new interface driver usbhid
[Mon Oct 16 09:45:39.530 2023] [ 1.695566] usbhid: USB HID core driver
[Mon Oct 16 09:45:39.530 2023] [ 1.708759] mmc0: Switching to 1.8V signalling voltage failed
[Mon Oct 16 09:45:39.530 2023] [ 1.710442] NET: Registered protocol family 10
[Mon Oct 16 09:45:39.530 2023] [ 1.721324] mmc0: new DDR MMC card at address 0001
[Mon Oct 16 09:45:39.530 2023] [ 1.721967] Segment Routing with IPv6
[Mon Oct 16 09:45:39.530 2023] [ 1.728844] mmcblk0: mmc0:0001 G1M15L 29.6 GiB
[Mon Oct 16 09:45:39.530 2023] [ 1.730087] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[Mon Oct 16 09:45:39.530 2023] [ 1.736182] mmcblk0boot0: mmc0:0001 G1M15L partition 1 31.5 MiB
[Mon Oct 16 09:45:39.530 2023] [ 1.742090] NET: Registered protocol family 17
[Mon Oct 16 09:45:39.530 2023] [ 1.748051] mmcblk0boot1: mmc0:0001 G1M15L partition 2 31.5 MiB
[Mon Oct 16 09:45:39.530 2023] [ 1.750984] can: controller area network core (rev 20170425 abi 9)
[Mon Oct 16 09:45:39.531 2023] [ 1.763556] NET: Registered protocol family 29
[Mon Oct 16 09:45:39.531 2023] [ 1.763663] mmcblk0rpmb: mmc0:0001 G1M15L partition 3 4.00 MiB, chardev (244:0)
[Mon Oct 16 09:45:39.531 2023] [ 1.768037] can: raw protocol (rev 20170425)
[Mon Oct 16 09:45:39.531 2023] [ 1.779992] can: broadcast manager protocol (rev 20170425 t)
[Mon Oct 16 09:45:39.536 2023] [ 1.785760] can: netlink gateway (rev 20170425) max_hops=1
[Mon Oct 16 09:45:39.536 2023] [ 1.791174] mmcblk0: p1 p2
[Mon Oct 16 09:45:39.536 2023] [ 1.791848] Key type dns_resolver registered
[Mon Oct 16 09:45:39.536 2023] [ 1.803437] Registering SWP/SWPB emulation handler
[Mon Oct 16 09:45:39.536 2023] [ 1.811018] Loading compiled-in X.509 certificates
[Mon Oct 16 09:45:39.559 2023] [ 1.875905] imx_thermal 20c8000.anatop:tempmon: Automotive CPU temperature grade - max:125C critical:120C passive:115C

 

Best regards,

Aryz.

 

 

 

 

 

0 Kudos
Reply
0 Replies