GPT timer lower count ISR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPT timer lower count ISR

2,021件の閲覧回数
manuel_iglesias
Contributor II

I am trying to generate a GPT interrupt as fast as possible, using the example code, the GPT clock source is 62.5MHz but I can only get an interrupt every 1us (not exactly as comparison count is 62 or 63 . If I specify a smaller compare value, the interrupt didn't seem to be triggering. Does anyone know if there is a limitation here?


Can it be possible to use a high speed internal clock, I have tried to change to the high frequency clock without seeing a difference. I might be missing some synchronization or something while trying to enable it.

I will appreciate any help,

Thanks,

タグ(1)
0 件の賞賛
返信
1 返信

1,933件の閲覧回数
lucas_cao
NXP Employee
NXP Employee

Hello,

May I know What did you do during the interruption process and how to get the signal of the interrupt has been generated?

Lucas Cao

0 件の賞賛
返信