FreeMASTER

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeMASTER

4,072件の閲覧回数
vladimir136
Contributor I

Hi,

Can FreeMASTER be used with i.MXRT1010 chip and MIMXRT1010-EVK tools?

Vladimir

0 件の賞賛
返信
3 返答(返信)

3,885件の閲覧回数
wesson_ding
NXP Employee
NXP Employee

We already have an RT1010 motor control project integrated with FreeMaster now.

You can find the Application Note with its software in the below link:

https://www.nxp.com/docs/en/application-note/AN12591.pdf 

The FreeMaster project is under the following path:

AN12591SW\src\common\motor_control\freemaster

You should following the steps in AN12591 if you want to drive the motor with freemaster,

pastedImage_2.png

Regards,

Wesson

0 件の賞賛
返信

3,884件の閲覧回数
philip_drake
NXP Employee
NXP Employee

Freemaster can be used with the i.MXRT1010 chip and the EVK. There are application notes that describe how to integrate Freemaster into any project. Check the Freemaster page for information.

Unfortunately the RT1010 SDK does not have the Freemaster tool integrated in the middleware package yet. 

If you would like to experiment you could down

1) download Freemaster and integrate it directly

2) download the i.MXRT1020 SDK, selecting the Freemaster and Motor control.  You could then port the code to RT1010.

Regards,

Philip

0 件の賞賛
返信

3,885件の閲覧回数
SanyaadeAdekoya
Contributor I

FreeMaster as I believe is an Eclipse base environment. Is there available source of its core to extend/customise.

Looks like a good platform to explore

0 件の賞賛
返信