[88W9098] - Do this module can support openwrt ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[88W9098] - Do this module can support openwrt ?

1,580件の閲覧回数
OttoLee
Contributor I

Hi NXP community :

    We have new production , and will use wifi module(use 88W9098 DB CDW 2x2 802.11ax, Bluetooth 5.1) 

     and we got the source code from "PCIE-WLAN-UART-BT-9098-U16-X86-17.68.1.p38-17.26.1.p38-MXM4X17222.P1_V0V1-GPL" , and we try to merge to Openwrt system , but encounter difficulty , it's hard to merge .

      I check Makefile and find below 

     # OpenWrt support
     CONFIG_OPENWRT_SUPPORT=n
     

    Does this mean not support for openwrt system ?

    And if I can generate *.ko  on Linux system first, then push these *.ko file to embedded system ?

Thanks

0 件の賞賛
返信
0 返答(返信)