88W8997 USB BT on Android 9

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

88W8997 USB BT on Android 9

3,390 Views
rahmanuh
Contributor III

Hello,

I notice these errors when trying to turn on BT from Android GUI. And it seems these are the root cause? It says that it is missing adapter section in bt_config.conf.

Anyone ever experienced such a case? How to solve it?

These are the errors:
09-22 11:49:06.835 4442 4459 E bt_btif_config: Config is missing adapter section
09-22 11:49:06.835 4442 4459 W bt_btif_config: init unable to load config file: /data/misc/bluedroid/bt_config.conf; using backup.
09-22 11:49:06.835 4442 4459 E bt_btif_config: Config is missing adapter section
09-22 11:49:06.835 4442 4459 W bt_btif_config: init unable to load backup; attempting to transcode legacy file.
09-22 11:49:06.835 4442 4459 E bt_btif_config_transcode: btif_config_transcode unable to load XML file '/data/misc/bluedroid/bt_config.xml': 3
09-22 11:49:06.835 4442 4459 E bt_btif_config: init unable to transcode legacy file; creating empty config.

Thank you in advance.

Best regards,
Rahmanu

0 Kudos
Reply
2 Replies

3,200 Views
rahmanuh
Contributor III

Hi Asma,

Yes. Please try to rebuild your Android with "#define BLE_VND_INCLUDED TRUE" in your bdroid_buildcfg.h.

Best regards,
Rahmanu

0 Kudos
Reply

3,204 Views
asmaa
Contributor V

Hi Rahmanuh,

 

Were you able to resolve the issue? I also getting same error.

 

Thanks,

Asma

0 Kudos
Reply