8080 Interface on IMX7SABRESD with yocto bsp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

8080 Interface on IMX7SABRESD with yocto bsp

1,178件の閲覧回数
pmpal19
Contributor I

Hi everyone. I'm trying to build an image for IMX7SABRESD which supports 8080 interface with the imx-yocto-bsp. I've tried this thread:
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Patch-to-support-MPU-8080-LCD-on-iMX6UL-...

as a starting point but I've had no luck using the patches listed. At the bottom of the thread someone updated the patch for kernel version imx_4.9.11_1.0.0_ga. I tried using that with the same version I found on:
https://source.codeaurora.org/external/imx/imx-manifest/

but still no luck. Can anyone help point me in the right direction? Or point me towards where I can look at the code for a linux mpu driver? Thanks.

0 件の賞賛
返信
0 返答(返信)