Setting BMS772

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting BMS772

Jump to solution
2,940 Views
Auvidea-AS
Contributor I

Hello,

We connected

 NXP-BMS772 (J3) with actual firmware from git to

orange cube (can1) with PX4 Pro v1.14.3.

On CAN we logged 18 frames per second but in QGroundControl the LiPo pack is not visible ?

Are there any setting required ?

PS:

Can log with HL-340 ( 1000000 Baud )

82.096391 dlc=4 0139041f 00 00 00 df
82.147965 dlc=8 0139041f 3c 35 f6 00 00 f8 00 00
82.149184 dlc=8 0139041f 00 f7 ff df fe 00 00 00
82.195299 dlc=2 01204e10 00 f7
82.196054 dlc=4 0139041f 00 f8 00 df
82.297600 dlc=4 0139041f 00 00 00 df
82.396399 dlc=4 0139041f 00 f8 00 df
82.406055 dlc=8 01550110 59 02 00 00 00 00 00 00
82.407121 dlc=8 01040001 88 f2 cd 23 00 00 00 00
82.495493 dlc=4 0139041f 00 00 00 23
82.597262 dlc=4 0139041f 00 f8 00 23
82.645951 dlc=8 0139041f 3c 35 f6 00 00 f8 00 00
82.647112 dlc=8 0139041f 00 f7 ff df fe 00 00 00
82.696385 dlc=2 01204e10 00 f7
82.697188 dlc=4 0139041f 00 00 00 df
82.795498 dlc=4 0139041f 00 f8 00 df
82.897469 dlc=4 0139041f 00 00 00 df
82.996337 dlc=4 0139041f 00 f8 00 df

 

0 Kudos
Reply
1 Solution
2,902 Views
GeraldP
NXP Employee
NXP Employee

You need to use the latest BMS reference SW, BMS release version 6 that was just released to have DroneCAN support.
It's available as https://github.com/NXPHoverGames/RDDRONE-BMS772/tree/main
The github documentation has been updated accordingly.

To get droneCAN running the following parameters needs to be set via console:
bms set can-mode DRONECAN
bms set dronecan-node-static-id 31
bms set dronecan-bat-info 1
bms set dronecan-bat-info-aux 1

View solution in original post

0 Kudos
Reply
3 Replies
2,903 Views
GeraldP
NXP Employee
NXP Employee

You need to use the latest BMS reference SW, BMS release version 6 that was just released to have DroneCAN support.
It's available as https://github.com/NXPHoverGames/RDDRONE-BMS772/tree/main
The github documentation has been updated accordingly.

To get droneCAN running the following parameters needs to be set via console:
bms set can-mode DRONECAN
bms set dronecan-node-static-id 31
bms set dronecan-bat-info 1
bms set dronecan-bat-info-aux 1

0 Kudos
Reply
1,952 Views
cisvmierlo
NXP Employee
NXP Employee

Hi,

Please also see How to integrate RDDRONE-BMS or MR-BMS771 in PX4 via DroneCAN | RDDRONE-BMS772 for the step by step guide including QGroundControl configuration.

Kind regards!

0 Kudos
Reply
2,887 Views
Auvidea-AS
Contributor I

thank you, now it works.

 

0 Kudos
Reply