PX4 Firmware problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,718件の閲覧回数
ArifKamal
Contributor I

After installing the bootloader and firmware recommended by gitbook, i have been unable to proceed through the QGroundControl app. It states that the Firmware is not supported or has a bug. i have repeatedly tried to reinstalled the bootloader and firmware but still comes out the same. Is there a way to get through this problem?

Screenshot 2021-06-12 022934.pngScreenshot 2021-06-12 022934.png

Screenshot 2021-06-12 020429.pngScreenshot 2021-06-12 020429.png

  

ラベル(2)
0 件の賞賛
返信
1 解決策
4,712件の閲覧回数
dk7xe
Contributor II

Please give is a try with just flashing the bootloader via the Segger programming Tool. My guess is that you are programming PX4 FW over the bootloader. PX4 FW needs to be programmed starting at adress 6000.

Therefore the easiest way is to just program the bootloader via the segger Tool. Reboot the FMU afterwards (Power cycle).

Only after that connect it to your PC having QGC at the FW Flash page.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,713件の閲覧回数
dk7xe
Contributor II

Please give is a try with just flashing the bootloader via the Segger programming Tool. My guess is that you are programming PX4 FW over the bootloader. PX4 FW needs to be programmed starting at adress 6000.

Therefore the easiest way is to just program the bootloader via the segger Tool. Reboot the FMU afterwards (Power cycle).

Only after that connect it to your PC having QGC at the FW Flash page.

0 件の賞賛
返信