PWM Outputs on RDDRONE-FMUK66

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PWM Outputs on RDDRONE-FMUK66

2,637件の閲覧回数
Kade98002
Contributor I

How many PWM outputs does the RDDRONE FMUK66 hardware kit support ? I have a VTOL with 4 motors and 5 servos. Can this kit control up to 9 motors ?

ラベル(1)
0 件の賞賛
返信
1 返信

2,606件の閲覧回数
iaingalloway
NXP Employee
NXP Employee

RevD of the RDDRONE-FMUK66 has 6 PWM outputs.
RevE is in progress and it will have 8 PWM outputs.

NOTE:
NXP UCANS32K146-01 is a UAVCANv1 Development board - it has two PWM outputs and also runs PX4 internally.
It could be used to add more PWM channels (and sensor inputs etc.)
UAVCANv1 is in its infancy, and as of today external PWM are not supported "turnkey" yet, but they will be.
Currently UAVCANv1 has a GPS example and a BMS example.

0 件の賞賛
返信