What is the size of RDDRONE-BMS772?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the size of RDDRONE-BMS772?

1,777 Views
Donghyun
Contributor I

What is the specifc frame size of RDDRONE-BMS772?

2 Replies

1,740 Views
iaingalloway
NXP Employee
NXP Employee

Thanks!
Since it is for development, It's designed to be able to zip-tie strap permanently to a LiPo battery that is typiclaly 3-4S 4000-5000mAh
One could also make a 3d printed case for the board and battery.

0 Kudos

1,746 Views
seongyooncho
Contributor I

It's 48 mm x 90.5 mm.