start up with external oscillator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

start up with external oscillator

1,908 Views
matthiasuhlmann
Contributor II

hi all,

is there a code example how to configure occs if external Crystal oscillator is used?

Labels (1)
0 Kudos
Reply
2 Replies

1,762 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

can you tell me the part number of DSC you are using? anyway, I suggest you use PE to generate the code to use external crystal or clock source, you can select the external crystal in cpu beans.

Hope it can help you

BR

XiangJun rong

0 Kudos
Reply

1,762 Views
matthiasuhlmann
Contributor II

Hi XiangJun rong,

I do not use Processor Expert. Would this generate a useful example?

I will try to generate example....

Thank you

BR

Matthias

0 Kudos
Reply