frequency settings influence the ADC result

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

frequency settings influence the ADC result

1,619 Views
andreasvogt
Contributor I

Hi,

 

i have a MC56F84769 controller. My bus clock is 50Mhz.

In the register ADC16_CFG1 I can select the clock divide settings (see below). The data sheet specifies that I need for 12Bit mode to keep inside 1.0 — 18.0Mhz.

If I change the divider settings between 4 and 8 during conversion my result changes although I am within the specified frequency.

Any ideas?

 

 

 

 

(00 The divide ratio is 1 and the clock rate is input clock.

01 The divide ratio is 2 and the clock rate is (input clock)/2.

10 The divide ratio is 4 and the clock rate is (input clock)/4.

11 The divide ratio is 8 and the clock rate is (input clock)/8.)

Labels (1)
0 Kudos
Reply
1 Reply

1,528 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Andreas,

As the following Fig in data sheet of MC56F847xx, the higher the ADC clock frequency, the less the ENOB spec, accordingly more the noise is. For high accuracy, pls decrease the ADC clock frequency to 1MHz.

Hope it can help you.

BR

Xiangjun Rong

pastedImage_0.png

0 Kudos
Reply