flasg over jtag in linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flasg over jtag in linux

Jump to solution
3,043 Views
cabl
Contributor III

Hi everybody,

 

has anyone tried to flash a S-record file to a DSP56F80X using a parallel command converter using Linux (Ubuntu)? Any helping tools? Any porting of flash_over_jtag?

 

BR,

Labels (1)
0 Kudos
Reply
1 Solution
2,880 Views
TICS_Fiona
NXP Employee
NXP Employee

flah_over_jtag only  runs under 32-bit Windows operating systems. It does not support Linux OS.

I attached this tool, help doc and its source code for your reference.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,881 Views
TICS_Fiona
NXP Employee
NXP Employee

flah_over_jtag only  runs under 32-bit Windows operating systems. It does not support Linux OS.

I attached this tool, help doc and its source code for your reference.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply