enumerate the USB host functionality

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

enumerate the USB host functionality

2,263件の閲覧回数
kishorravi
Contributor I

Hai, all,

some times you feel i am asking some thing strange,But i am tied with a problem associated with the subject.

Is there any possibility to enumerate the USB host functionality inside a processor with out USB peripheral. If so please give some open source example/ USB stack / Third party stack (for other device) with the HOST ability. My micro controller is MC56F8037. Any updates or hinds in above subject is a great help for me!!!!!.

2 返答(返信)

2,153件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Kishor

it is impossible to use GPIO pins as USB host interface. On the MC56F8037 Demo board, there is a USB-uart bridge IC called CP2102, but the CP2102 can be only a device rather than a host.
you can use the kinetis family with on-chip USB module as USB host, and MC56F8037 can communicate with the Kinmetis via spi, uart...
BTW, you can use the Kinetis family with USB module/PWM/ADC/timer modules to develop UPS.
For kinetis, we have developed the usb stack for both host/device.
Hope it can help you.

BR

Xiangjun Rong

2,153件の閲覧回数
kishorravi
Contributor I

Hi Xiangjun.rong

I also go through some researches and i also reach the same point.We are planning for scaling up of the processor. 

Thank you for your help.

Kishor R

0 件の賞賛
返信