code was deleted from build(MC56F84766 w/CW10.6)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

code was deleted from build(MC56F84766 w/CW10.6)

4,633件の閲覧回数
EngHuiPeng
NXP Employee
NXP Employee

Customer run on the same source code for MC56F84766 with the same CW 10.6 but different system. It was found that one of the system have a line containing S307020000000000F6 has been removed. What could be the scenario that could cause this line being deleted. Enclosed is the S record comparison.

 

Regards,

Audrey

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

4,332件の閲覧回数
EngHuiPeng
NXP Employee
NXP Employee

Fiona,

Are you referring to the DSC linker option?

If so, the same setting are being used.

The only difference that the one that do not got deleted is using Drive C and the one that got deleted is on Drive D. Don't think that could cause the issue right?

Regards,

Audrey

0 件の賞賛
返信

4,332件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Hui Peng

Below is the description for S-record format.

http://www.sbprojects.com/knowledge/fileformats/motorola.php

It seems that S307020000000000F6 does not contain any valid data. Because it is an address in Data RAM. It should be removed from S-record file.

Please compare the MAP file of these two projects. If the MAP files are same, then compare the version of linker.

Best Regards

Fiona Kuang

TIC - Technical Information Center

0 件の賞賛
返信

4,332件の閲覧回数
EngHuiPeng
NXP Employee
NXP Employee

Fiona,

MAP files are the same

Where do I find the linker version?

Is the linker inside CW installation folder?

Regards,

Audrey

0 件の賞賛
返信

4,332件の閲覧回数
johnlwinters
NXP Employee
NXP Employee

I would check these things from most to least likely:

1. Do both systems have the same set of updates to CW 10.6 installed?

2. Are the options in the projects set identically?

3. Is the java version on the system the same?

4. Is the OS the same on both computers with the same updates (this is least likely cause).

0 件の賞賛
返信

4,332件の閲覧回数
EngHuiPeng
NXP Employee
NXP Employee

John,

Following is the answer to your questions:

1. Do both systems have the same set of updates to CW 10.6 installed? Yes

2. Are the options in the projects set identically? Project setting should be the same as it came from SVN

3. Is the java version on the system the same? The one that have issue is V6 and the one that have no issue is V8 but when the refresh both to V8, the problem still exist

4. Is the OS the same on both computers with the same updates (this is least likely cause). Both Win7

0 件の賞賛
返信